imxg2dcompositor|imxipucompositor not support appsrc?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxg2dcompositor|imxipucompositor not support appsrc?

ソリューションへジャンプ
1,932件の閲覧回数
adorable
Contributor III

I want to use appsrc|appsink to push frame-data to imxg2dcompositor or imxipucompositor,but I found the compositor not support appsrc, the error is :internel data streamer err in appsrc.

If I want to use appsink|appsrc to video-compositor,how should I do?

kernel 4.9.88 Imx6q gstreamer1.12.2

0 件の賞賛
返信
1 解決策
1,912件の閲覧回数
adorable
Contributor III

phy continues and count not user appsink to push data to appsrc.

Finally I modifyed  imxipuvideotransform to modify frame-buffer ,and successed to compositor video0 and video1.video0 is parsed as RGBA,video1 is parsed as I420.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,913件の閲覧回数
adorable
Contributor III

phy continues and count not user appsink to push data to appsrc.

Finally I modifyed  imxipuvideotransform to modify frame-buffer ,and successed to compositor video0 and video1.video0 is parsed as RGBA,video1 is parsed as I420.

0 件の賞賛
返信
1,922件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Please refer to this example code to use ipuhttps://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_ipudev_test?h=imx_4.14.98_2.1.0 

 

BR

Zhiming

0 件の賞賛
返信