imxfb: No graphics output until XOrg was started

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imxfb: No graphics output until XOrg was started

2,017 次查看
stkoch
Contributor I

Hi,

I have ported Linux 3.7-rc4 to an board with an i.MX257 CPU. A display is connected via LVDS.

The used distribution is Debian Sqeeze for armel.

Until I have started XOrg I have no output on screen, no Linux Tux symbol and no text console.

If I start XOrg I have a correct output, when I terminate XOrg I have an text console.

How to show the Linux Tux and/or the Text console before XOrg starts?

The kernel command line includes "video=imxfb:LCD-SVGA-10-4".

Is another command line string necessary?

Thanks

Stefan Koch

标签 (3)
0 项奖励
回复
5 回复数

1,801 次查看
YixingKong
Senior Contributor IV

Stefan

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

1,801 次查看
andrew_questps
Contributor III

I'm pretty sure that it is a build option for the kernel under drivers->graphics support->bootup logo to enable the Tux, and there is another option near there to enable the text console.

0 项奖励
回复

1,801 次查看
stkoch
Contributor I

Thank you.

Both options are still enabled.

The black screen must be another issue.

Is fbcon the module that shows the Tux and boot messages - or show's it only the login prompt?

With black screen there is no vsync and hsync signal.

This will enabled first when starting X11.

What could be the issue?

Thank you

0 项奖励
回复

1,801 次查看
YixingKong
Senior Contributor IV

Stefan

We have not got your response yet and will close the diacussion in 3 days. If you still need help, please feel free to

reply with an update to this discussion.
Thanks,
Yixing

0 项奖励
回复

1,801 次查看
YixingKong
Senior Contributor IV

Stefan

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.

Thanks,

Yixing

0 项奖励
回复