imxRT1176 Reinitializing flexspi causes MCU to restart

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxRT1176 Reinitializing flexspi causes MCU to restart

788件の閲覧回数
xiaozezitian
Contributor I

I use the imxRT1176 MCU.When both cores are used, the M7 core is used as the main core and the M4 core is used as the slave core. If flexspi is initialized in the M7 core and then deinit flexspi, and after starting the M4 core, flexspi is reinitialized in the M4 core, which causes the MCU to restart. What is the reason for this? How can I still use flexspi in the M4 core after initializing flexspi in the M7 core.

0 件の賞賛
返信
1 返信

758件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @xiaozezitian,

I believe this is a duplicated post from the following: https://community.nxp.com/t5/i-MX-Processors/imxRT1176-if-flash-is-to-be-erased-all-interrupts-of-bo...

I have already provided follow-up on the linked community post in order to prevent double efforts.

BR,
Edwin.

0 件の賞賛
返信