imx93evk /dev/ttyLP4 is not created for Bluetooth

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx93evk /dev/ttyLP4 is not created for Bluetooth

跳至解决方案
1,425 次查看
Chihyu_Lin
Contributor III

IMX93EVK default setting with iw612 UART Bluetooth using lpuart5, but /dev/ttyLP4 was not enable. 

[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw
[ 0.870871] 44380000.serial: ttyLP0 at MMIO 0x44380010 (irq = 18, base_baud = 1500000) is a FSL_LPUART
[ 0.880228] printk: console [ttyLP0] enabled
[ 0.905456] 42590000.serial: ttyLP4 at MMIO 0x42590010 (irq = 19, base_baud = 1500000) is a FSL_LPUART
[ 0.914849] serial serial0: tty port ttyLP4 registered

0 项奖励
回复
1 解答
1,379 次查看
Chihyu_Lin
Contributor III

Thanks for your reply, I had found a document about new kernel BT UART setting. The problem is solved.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Bluetooth-NXP-UART-Driver-Linux-BSP-6-1-...

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,394 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @Chihyu_Lin

Could you please tell me your BSP version?

Also, I suggest using the iMX Linux User's Guide of your BSP version and use the commands provided in the section Connectivity to effectively use the Bluetooth driver.

Here is a link to iMX Linux User's Guide from our latest BSP release: i.MX Linux User's Guide (nxp.com)

Have a great day!

0 项奖励
回复
1,380 次查看
Chihyu_Lin
Contributor III

Thanks for your reply, I had found a document about new kernel BT UART setting. The problem is solved.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Bluetooth-NXP-UART-Driver-Linux-BSP-6-1-...

0 项奖励
回复