Hi, guys,
my own board would not boot at all. the following is from reference pdf.

I find the mode1 pin is different from other 3 pin.
if we set DIP SW as 0000. the pin voltage level the the for pin is:
mode3 mode2 mode1 mode0 is:
low low high low. (voletage level)
my description is OK?
and second issue. to simple the design. and fix the board boot from emmc
0000.
I pull down all the for pin(mode3 to mode0) to low level volatage with 100K.
after one second, I switch the mode0 pin to UART purpose. (boot procedure finished). I wish I would see the uart logs and control the board.
but I see nothing.
what happend?
would you please help me ?