imx93: SRK revocation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx93: SRK revocation

ソリューションへジャンプ
2,263件の閲覧回数
mothacehe
Contributor I

Hello,

I am trying to perform key revocation on my closed imx93 board.

My CSF file looks like:

[Header]
Target = AHAB
Version = 1.0

[Install SRK]
File = "../cst-3.4.0/crts/SRKtable.bin"
Source = "../cst-3.4.0/crts/SRK2_sha384_secp384r1_v3_usr_crt.pem"
Source index = 1
Source set = OEM
Revocations = 0x1

[Authenticate Data]
File = "spl.bin"
Offsets = 0x400 0x490

The idea is to sign with SRK2 and revoke SRK1 (0x1 bitmask). Booting from that image works fine, but I can still also boot from an image signed with SRK1.

Is there anything else that needs to be done in order to revoke SRK1?

Thanks,

Mathieu

0 件の賞賛
返信
1 解決策
2,214件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

check if missing the step ahab_commit 0x10

 

Regards

Harvey

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,215件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

check if missing the step ahab_commit 0x10

 

Regards

Harvey

0 件の賞賛
返信
2,205件の閲覧回数
mothacehe
Contributor I

That worked thanks. I had to add support for ahab_commit mainline though: https://lists.denx.de/pipermail/u-boot/2024-March/548873.html

0 件の賞賛
返信