imx93 EVK ONOFF button not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx93 EVK ONOFF button not working

跳至解决方案
869 次查看
marekb
Contributor III

Hi, I'm using imx93 evk with yocto build NXP i.MX Release Distro 6.6-nanbield imx93-11x11-lpddr4x-evk ttyLP0 release. I'm trying to power off/on board using ON/OFF button but it doesn't work.

Button send an events:

oot@imx93-11x11-lpddr4x-evk:~# evtest /dev/input/event0
Input driver version is 1.0.1
Input device ID: bus 0x19 vendor 0x0 product 0x0 version 0x0
Input device name: "44440000.bbnsm:pwrkey"
Supported events:
Event type 0 (EV_SYN)
Event type 1 (EV_KEY)
Event code 116 (KEY_POWER)
Properties:
Testing ... (interrupt to exit)
Event: time 1714639992.867395, type 1 (EV_KEY), code 116 (KEY_POWER), value 1
Event: time 1714639992.867395, -------------- SYN_REPORT ------------
Event: time 1714639992.995415, type 1 (EV_KEY), code 116 (KEY_POWER), value 0
Event: time 1714639992.995415, -------------- SYN_REPORT ------------
Event: time 1714639993.927423, type 1 (EV_KEY), code 116 (KEY_POWER), value 1
Event: time 1714639993.927423, -------------- SYN_REPORT ------------
Event: time 1714639994.055420, type 1 (EV_KEY), code 116 (KEY_POWER), value 0
Event: time 1714639994.055420, -------------- SYN_REPORT ------------
Event: time 1714639994.667422, type 1 (EV_KEY), code 116 (KEY_POWER), value 1

Thanks.

 

标记 (1)
0 项奖励
回复
1 解答
817 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Please try to hold the button about 5s.

在原帖中查看解决方案

0 项奖励
回复
1 回复
818 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Please try to hold the button about 5s.

0 项奖励
回复