imx8x reserved-memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8x reserved-memory

1,245 Views
songhongliang
Contributor II

I set the reserved memory in the dts. I only reserved dozens of megabytes of memory, but the kernel log shows that more than 200 megabytes of memory are reserved, imx8x. Is there any other place besides the dts set the reserved memory

log:

[ 0.000000] Memory: 492256K/1046528K available (18560K kernel code, 1558K rwdata, 7180K rodata, 3840K init, 544K bss, 226592K reserved, 327680K cma-reserved)

dtb->dts:

reserved-memory {
#address-cells = <0x02>;
#size-cells = <0x02>;
ranges;

decoder-boot@0x84000000 {
reg = <0x00 0x84000000 0x00 0x2000000>;
no-map;
phandle = <0x40>;
};

encoder-boot@0x86000000 {
reg = <0x00 0x86000000 0x00 0x200000>;
no-map;
phandle = <0x43>;
};

decoder-rpc@0x86200000 {
reg = <0x00 0x86200000 0x00 0x100000>;
no-map;
phandle = <0x41>;
};

encoder-rpc@0x94400000 {
reg = <0x00 0x94400000 0x00 0x700000>;
no-map;
phandle = <0x44>;
};

linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0x00 0x14000000>;
alloc-ranges = <0x00 0x98000000 0x00 0x14000000>;
linux,cma-default;
};
};

0 Kudos
Reply
1 Reply

1,224 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Please refer to Chapter 7 Memory Assignment and Table 1. DDR memory assignment in i.MX Porting Guide, where DRAM memory regions are reserved for ATF, SCFW, etc...
 
One can also try to debug with the below sysfs directory to cross-check if any overlay is not applied to device tree.
$ cd sys/firmware/devicetree/base/reserved-memory/
$ ls
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply