imx8x reserved-memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8x reserved-memory

1,611件の閲覧回数
songhongliang
Contributor II

I set the reserved memory in the dts. I only reserved dozens of megabytes of memory, but the kernel log shows that more than 200 megabytes of memory are reserved, imx8x. Is there any other place besides the dts set the reserved memory

log:

[ 0.000000] Memory: 492256K/1046528K available (18560K kernel code, 1558K rwdata, 7180K rodata, 3840K init, 544K bss, 226592K reserved, 327680K cma-reserved)

dtb->dts:

reserved-memory {
#address-cells = <0x02>;
#size-cells = <0x02>;
ranges;

decoder-boot@0x84000000 {
reg = <0x00 0x84000000 0x00 0x2000000>;
no-map;
phandle = <0x40>;
};

encoder-boot@0x86000000 {
reg = <0x00 0x86000000 0x00 0x200000>;
no-map;
phandle = <0x43>;
};

decoder-rpc@0x86200000 {
reg = <0x00 0x86200000 0x00 0x100000>;
no-map;
phandle = <0x41>;
};

encoder-rpc@0x94400000 {
reg = <0x00 0x94400000 0x00 0x700000>;
no-map;
phandle = <0x44>;
};

linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0x00 0x14000000>;
alloc-ranges = <0x00 0x98000000 0x00 0x14000000>;
linux,cma-default;
};
};

0 件の賞賛
返信
1 返信

1,590件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Please refer to Chapter 7 Memory Assignment and Table 1. DDR memory assignment in i.MX Porting Guide, where DRAM memory regions are reserved for ATF, SCFW, etc...
 
One can also try to debug with the below sysfs directory to cross-check if any overlay is not applied to device tree.
$ cd sys/firmware/devicetree/base/reserved-memory/
$ ls
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信