imx8ulp misc gpio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8ulp misc gpio

1,280件の閲覧回数
tangchao90
Contributor III

I now want to design a program to determine whether a pull-up resistor exists!

below pins: onoff, tamper0, tamper1, reset and so on

but i do not how to control these

1739330804046.png

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,268件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

If my understanding is correct, you want to use program to operate misc gpios(output/input/set high/set low) to check whether a pull-up resistor exists. Is that correct?



Best Regards,
Zhiming

0 件の賞賛
返信

1,251件の閲覧回数
tangchao90
Contributor III

yes!

0 件の賞賛
返信

1,236件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

The ONOFF, tamper0, tamper1, reset is not standard GPIO, these io has special function which could affect system running. We don't recommend you use these IO in your program.

Best Regards,
Zhiming

0 件の賞賛
返信