imx8ulp misc gpio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8ulp misc gpio

1,281 Views
tangchao90
Contributor III

I now want to design a program to determine whether a pull-up resistor exists!

below pins: onoff, tamper0, tamper1, reset and so on

but i do not how to control these

1739330804046.png

Labels (1)
0 Kudos
Reply
3 Replies

1,269 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

If my understanding is correct, you want to use program to operate misc gpios(output/input/set high/set low) to check whether a pull-up resistor exists. Is that correct?



Best Regards,
Zhiming

0 Kudos
Reply

1,252 Views
tangchao90
Contributor III

yes!

0 Kudos
Reply

1,237 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

The ONOFF, tamper0, tamper1, reset is not standard GPIO, these io has special function which could affect system running. We don't recommend you use these IO in your program.

Best Regards,
Zhiming

0 Kudos
Reply