[imx8qxpmek ][Yocto] Use sstate in yocto getting error.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[imx8qxpmek ][Yocto] Use sstate in yocto getting error.

1,745 次查看
WolsYang
Contributor IV

Hi NXP,

I am trying to use sstate to increase build speed and reduce the disk space needed.

First, create a clean build.

DISTRO=fsl-imx-wayland MACHINE=imx8qxpc0mek source imx-setup-release.sh -b build

Then edit build/conf/local.conf

SSTATE_DIR ?="/share/yocto-sstate/"

And build, all good.

bitbake imx-image-multimedia

But the other build tries to use the same sstate getting an error.

DISTRO=fsl-imx-wayland MACHINE=imx8qxpc0mek source imx-setup-release.sh -b build2

# build2/conf/local.conf
SSTATE_DIR ?="/share/yocto-sstate/"

#Then build
bitbake imx-image-multimedia

And getting error

ERROR: imx-image-multimedia-1.0-r0 do_rootfs: Error executing a python function in exec_func_python() autogenerated:

The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_func_python() autogenerated', lineno: 2, function: <module>
     0001:
 *** 0002:license_create_manifest(d)
     0003:
File: '/path/to/imx5.15.52/sources/poky/meta/classes/license_image.bbclass', lineno: 38, function: license_create_manifest
     0034:    pkg_dic = {}
     0035:    for pkg in sorted(image_list_installed_packages(d)):
     0036:        pkg_info = os.path.join(d.getVar('PKGDATA_DIR'),
     0037:                                'runtime-reverse', pkg)
 *** 0038:        pkg_name = os.path.basename(os.readlink(pkg_info))
     0039:
     0040:        pkg_dic[pkg_name] = oe.packagedata.read_pkgdatafile(pkg_info)
     0041:        if not "LICENSE" in pkg_dic[pkg_name].keys():
     0042:            pkg_lic_name = "LICENSE:" + pkg_name
Exception: FileNotFoundError: [Errno 2] No such file or directory: '/path/to/imx5.15.52/build2/tmp/pkgdata/imx8qxpc0mek/runtime-reverse/kernel-5.15.52+ga3a946ec1ef5'

ERROR: Logfile of failure stored in: /path/to/imx5.15.52/build2/tmp/work/imx8qxpc0mek-poky-linux/imx-image-multimedia/1.0-r0/temp/log.do_rootfs.3670757
ERROR: Task (/path/to/imx5.15.52/sources/meta-imx/meta-sdk/recipes-fsl/images/imx-image-multimedia.bb:do_rootfs) failed with exit code '1'

How can I fix it? 

0 项奖励
回复
2 回复数

1,726 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @WolsYang 

The problem seems not caused by sstate but dependencies files missed. you can try to edit DL_DIR using previous successful DL_DIR for source fetching.

 

Best regards

Harvey

0 项奖励
回复

1,723 次查看
WolsYang
Contributor IV

Hi @Harvey021 

In both build directories (build and build2) conf, they have the same download directory.

DL_DIR ?= "/media/wols/WOLSDATAHDD/imx5.15.52/downloads/"

After the error showed, I try to re-clean build in the build directory, and it is work fine.

That is why I think is not  DL_DIR problem.

0 项奖励
回复