imx8qxp spdif use error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp spdif use error

Jump to solution
1,805 Views
relax-wu
Contributor IV

Hi

CPU:imx8qx6avlf

SDK:Android Q10.0.0_2.2.0_AUTO

lunch mek_8q_car_userdebug

I don’t know much about alsa, now refer to imx8qxp-lpddr4-val-spdif.dts to modify.

devic-tree

sound-spdif {
    compatible = "fsl,imx-audio-spdif";
    model = "imx-spdif";
    spdif-controller = <&spdif0>;
    spdif-in;
    spdif-out;
};

driver:vendor/nxp-opensource/kernel_imx/sound/soc/fsl/fsl_spdif.c

Test steps:

mek_8q:/ # cat /proc/asound/cards
 0 [imxspdif       ]: imx-spdif - imx-spdif
                      imx-spdif
mek_8q:/ # ls dev/snd -l
total 0
crw-rw---- 1 system audio 116,   4 1970-01-01 00:00 controlC0
crw-rw---- 1 system audio 116,   3 1970-01-01 00:00 pcmC0D0c
crw-rw---- 1 system audio 116,   2 1970-01-01 00:00 pcmC0D0p
crw-rw---- 1 system audio 116,  33 1970-01-01 00:00 timer
mek_8q:/ #
mek_8q:/ # tinypcminfo -D 0 -d 0
Info for card 0, device 0:

PCM out:
      Access:   0x000009
   Format[0]:   0x000040
   Format[1]:   00000000
 Format Name:   S24_LE
   Subformat:   0x000001
        Rate:   min=32000Hz     max=192000Hz
    Channels:   min=2           max=2
 Sample bits:   min=32          max=32
 Period size:   min=32          max=8192
Period count:   min=2           max=2048

PCM in:
      Access:   0x000009
   Format[0]:   0x000040
   Format[1]:   00000000
 Format Name:   S24_LE
   Subformat:   0x000001
        Rate:   min=16000Hz     max=192000Hz
    Channels:   min=2           max=2
 Sample bits:   min=32          max=32
 Period size:   min=32          max=8192
Period count:   min=2           max=2048
mek_8q:/ #
mek_8q:/ # tinyplay /sdcard/1khz-48000-32-2.wav -p 1024 -r 3
Unable to open PCM device 0 (cannot set hw params: Invalid argument)
mek_8q:/ #

error log

Unable to open PCM device 0 (cannot set hw params: Invalid argument)
0 Kudos
Reply
1 Solution
1,758 Views
relax-wu
Contributor IV

This is the solution

View solution in original post

0 Kudos
Reply
3 Replies
1,759 Views
relax-wu
Contributor IV

This is the solution

0 Kudos
Reply
1,797 Views
igorpadykov
NXP Employee
NXP Employee

Hi relax-wu

 

supported interfaces are described in Android Release Notes, per this document seems spdif

is not supported, sorry. One can try to test it in linux:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
Reply
1,777 Views
relax-wu
Contributor IV

Has not yet reached the Android layer
Tinyplay operates the Linux driver directly, this step is a failure.

0 Kudos
Reply