I am investigating boot time optimizations and noticed there are a couple of fuses relating to mmc fast boot.
Our board is using an mmc 5.1 component so I believe it should be compatible with the requirements specified in the Application Process Manual 'Table 5-16. MMC and eMMC boot details'.
The two fuses that seem to be relevant to us are 'MMC Bus Width' and 'Fast Boot'. I am a bit hesitant to test these as I don't wish to blow fuses.
Is it possible to test this feature without blowing the fuses?