Hi guys,
I have a trouble thing about uuu flasing to emmc in imx8qxpmek evaluation board.
I have connected USB C type to imx8qxpmek and tried to flash images included in bootloader image.
my sequence is like below:
sudo uuu/uuu ./uuu.auto
and result is that :
1/1 [HID(W):LIBUSB_ERROR_IO ] SDPS: boot -f imx-boot-imx8qxpmetk-sd.bin-flash.
I am suspecting wrong bootloader image but, i have tried other bootlaoder imag such as (imx-boot-imx8qxpmek-sd , imx-boot-imx8qxpmek-sd.bin-flash_linux_m4, imx-boot-imx8qxpmek-sd.bin-flash_lregression_inux_m4), but all failed.
Do you have any idea to fix my issue?
Thanks,
Hi yibhan
one can look at below links for possible solutions:
https://community.nxp.com/t5/i-MX-Processors/imx8qxp-mek-uuu-fail/m-p/993787
https://community.nxp.com/t5/i-MX-Processors/IMX8QM-uuu-u-boot-Failed/m-p/832859
Best regards
igor
Hi guys,
I have a Imx8qxpmek rev C and I am using kernel 4.14.98.2.0.0, but it is always failed.
So, I have changed to imx8qxpmek 4.14.98_2.3.0 images and then download it and it is ok.
I have a question for it. Should I compile it for imx8qxpc0 ? if so, how do i compile it in yocto?
Do i use kernel 4.14.98.2.0.0 images for imx8qxpmek rev C?
>I have a Imx8qxpmek rev C and I am using kernel 4.14.98.2.0.0, but it is always failed.
kernel 4.14.98.2.0.0 does not support i.MX 8QuadXPlus (C0) MEK as described on below
link column "Supported Platforms"
Best regards
igor
>How should I build imx8qxpc0 yocto build in kernel 4.14.98_2.3.0?
it is the same as for kernel 4.14.98_2.0.0, for rev.C0 one needs to build SCFW with "R="
silicon revision option, described in SCFW Porting Kit
Best regards
igor
Hi guys,
I want to know how to build imx8qxpc0mek in yocto.
Do I just change MACHINE=imx8qxpc0mek or other thing is changed?
Could you please confirm below commands?
=================
$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m
imx-4.14.98-2.3.0.xml
$ repo sync
$ DISTRO=fsl-imx-xwayland MACHINE=imx8qxpc0mek source fsl-setup-release.sh -b build-xwayland
$ bitbake fsl-image-qt5-validation-imx
====================
yes MACHINE=imx8qxpc0mek is sufficient.
Best regards
igor