[imx8qxp]How to use pcie with internel clock?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[imx8qxp]How to use pcie with internel clock?

834 次查看
WolsYang
Contributor IV

Hi NXP,

I wish i can use internel pll clock with pcie, so I follow up this post to change SCFW and device-tree.

https://community.nxp.com/t5/i-MX-Processors/imx8q-PCIE-internal-clock-master/m-p/1155340

But still got error message like below, here is my dts pcie setting, is there anything I missied?

&pcieb{
    compatible = "fsl,imx8qxp-pcie","snps,dw-pcie";
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_pcieb>;
    disable-gpio = <&max7311 0 GPIO_ACTIVE_LOW>;
    reset-gpio = <&lsio_gpio4 0 GPIO_ACTIVE_LOW>;
    // clkreq-gpio = <&lsio_gpio4 1 GPIO_ACTIVE_LOW>;
    ext_osc = <0>;
    status = "okay";
};

 

[ 3.441546] imx6q-pcie 5f010000.pcie: supply epdev_on not found, using dummy regulator
[ 3.457451] imx6q-pcie 5f010000.pcie: No cache used with register defaults set!
[ 3.500102] imx6q-pcie 5f010000.pcie: PCIe PLL is locked.
[ 3.509138] imx6q-pcie 5f010000.pcie: iATU unroll: disabled
[ 3.514805] imx6q-pcie 5f010000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[ 3.522432] imx6q-pcie 5f010000.pcie: host bridge /bus@5f000000/pcie@0x5f010000 ranges:
[ 3.530549] imx6q-pcie 5f010000.pcie: IO 0x007ff80000..0x007ff8ffff -> 0x0000000000
[ 3.538775] imx6q-pcie 5f010000.pcie: MEM 0x0070000000..0x007fefffff -> 0x0070000000
[ 3.547149] imx6q-pcie 5f010000.pcie: iATU unroll: disabled
[ 3.552740] imx6q-pcie 5f010000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[ 4.552194] imx6q-pcie 5f010000.pcie: Phy link never came up
[ 4.558964] imx6q-pcie: probe of 5f010000.pcie failed with error -110

 

0 项奖励
回复
1 回复

817 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @WolsYang,

Could you please confirm which BSP version you are using?

 

Best Regards,
Dhruvit.

0 项奖励
回复