imx8qmmek flash without changing dip switches

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8qmmek flash without changing dip switches

跳至解决方案
1,063 次查看
ambrice
Contributor II

I have received i.MX8QM MEK board, put it into serial downloader mode, and flashed L5.4.47-2.2.0 release onto the emmc with uuu, and it boots up.  But changing those tiny dip switches back and forth to update to emmc is a pain.  I saw some posts suggesting "bmode usb" run in u-boot would make it switch to serial downloader mode, but there is no bmode command in the released u-boot.  I tried "ums 0 mmc 0" and "ums 1 mmc 0" but neither made the emmc show up as a usb disk over the usb-c connector.  Is there a way to flash the emmc without changing the boot mode switches?

0 项奖励
回复
1 解答
1,056 次查看
ambrice
Contributor II

It looks like "fastboot usb 1" is what I'm looking for

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,057 次查看
ambrice
Contributor II

It looks like "fastboot usb 1" is what I'm looking for

0 项奖励
回复