imx8qm lpddr4 android bsp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qm lpddr4 android bsp

ソリューションへジャンプ
745件の閲覧回数
Grigoriy
Contributor III

Hi!

I'm trying to flash a board from phytec with imx8qm on board. I've downloaded Android 14 from the nxp page. I tried to run uuu_imx_android_flash.sh script but it keeps failing with error:

[HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -f imx-boot-imx8qmmek-sd.bin-flash

The command was:

sudo ./uuu_imx_android_flash.sh -f imx8qm

 

As I understood the error is related to LPDDR4 and DDR4. The board has LPDDR4 and my question is the android build or uboot from the build don't support LPDDR4?

 

Also, tried to flash linux and got the same error.   

0 件の賞賛
返信
1 解決策
726件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

The problem is the imx-boot image, there must be differences other than the LPDDR4 because 8QM-MEK has a LPDDR4 memory. The differences in RAM configuration, channels of PMIC, memories, etc. cause failures probing, then failure booting an image specially with this SoC since the resources are managed by SCFW.

You have to use PHYTEC release of Android since it requires a lot of partitions and are checksum-ed, with Linux you could adapt working with our RootFS integrating PHYTEC imx-boot, device tree and probably Kernel image, the other option is to use PHYTEC Linux release too.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
727件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

The problem is the imx-boot image, there must be differences other than the LPDDR4 because 8QM-MEK has a LPDDR4 memory. The differences in RAM configuration, channels of PMIC, memories, etc. cause failures probing, then failure booting an image specially with this SoC since the resources are managed by SCFW.

You have to use PHYTEC release of Android since it requires a lot of partitions and are checksum-ed, with Linux you could adapt working with our RootFS integrating PHYTEC imx-boot, device tree and probably Kernel image, the other option is to use PHYTEC Linux release too.

Regards

0 件の賞賛
返信
696件の閲覧回数
Grigoriy
Contributor III
Hi,
Thank you for your answer!
0 件の賞賛
返信