imx8qm Xen Boot fails on hardware partition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm Xen Boot fails on hardware partition

7,433 Views
minskey_guo
Contributor II

I am working a customized imx8qm mek board, and run into trouble with hardware partition.   During uboot period, if "scu_rm dtb" is called,  the memory @ 0x85000000 cannot be accessed, as a result,  system reset when load Dom0 kernel to that address,   the details as follows:

=> fatload mmc 0:1 0x80280000 xen
819536 bytes read in 11 ms (71.1 MiB/s)
=> fatload mmc 0:1 0x83000000 fsl-imx8qm-mek-dom0.dtb
104201 bytes read in 9 ms (11 MiB/s)
=> scu_rm dtb 0x83000000
fdt addr 0000000083000000
partition_alloc: os_part, 4: parent_part, 3
=> scu_rm print
part id: 4 3
=> fatload mmc 0:1 0x85000000 Image
"Synchronous Abort" handler, esr 0x96000210
elr: 000000008004acdc lr : 000000008004accc (reloc)
elr: 00000000ffea6cdc lr : 00000000ffea6ccc
x0 : 00000000ffffffff x1 : 00000000fd66b320
x2 : 00000000fd66b308 x3 : 00000000ffea6c98
x4 : 000000000000000e x5 : 000000000000000e
x6 : 0000000000000000 x7 : 0000000000000010
x8 : 0000000000000044 x9 : 0000000000000008
x10: 00000000ffffffd8 x11: 0000000000000006
x12: 000000000001869f x13: 00000000000187ac
x14: 00000000fd66b70c x15: 00000000ffffffff
x16: 0000000000002080 x17: 0000000000000000
x18: 00000000fd679da8 x19: 000000005b010000
x20: 00000000fd684f50 x21: 00000000fd66b308
x22: 00000000fd66b320 x23: 0000000000000000
x24: 0000000000000000 x25: 00000000fd686970
x26: 00000000ffee346d x27: 0000000000000011
x28: 0000000000000001 x29: 00000000fd66b250

Resetting CPU ...

However, if I skip "scu_rm dtb 0x83000000 ",  Xen can boot but will panic later:

 

=> fatload mmc 0:1 0x80280000 xen
819536 bytes read in 11 ms (71.1 MiB/s)
=> fatload mmc 0:1 0x83000000 fsl-imx8qm-mek-dom0.dtb
104201 bytes read in 9 ms (11 MiB/s)
=> fatload mmc 0:1 0x85000000 Image
23175680 bytes read in 101 ms (218.8 MiB/s)
=> fdt addr 0x83000000
=> fdt resize 256
=> fdt set /chosen/module@0 reg <0x00000000 0x85000000 0x00000000 0x${filesize}>
=> fdt set /chosen/module@0 bootargs "${bootargs} ${xenlinux_bootargs}"
=> setenv bootargs ${xenhyper_bootargs};
=> booti ${loadaddr} - ${fdt_addr};
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
reserving fdt memory region: addr=84000000 size=2000000
reserving fdt memory region: addr=86000000 size=400000
reserving fdt memory region: addr=90000000 size=400000
reserving fdt memory region: addr=90400000 size=1c00000
reserving fdt memory region: addr=92000000 size=200000
reserving fdt memory region: addr=92400000 size=2000000
reserving fdt memory region: addr=83000000 size=1a000
Using Device Tree in place at 0000000083000000, end 000000008301cfff
/dma-controller@599F0000, 67608

Starting kernel ...

Xen 4.11.1-pre
(XEN) Xen version 4.11.1-pre (minskey@) (aarch64-poky-linux-gcc (GCC) 7.3.0) debug=n Wed May 22 14:49:04 UTC 2019
(XEN) Latest ChangeSet: Tue Apr 16 16:24:07 2019 +0800 git:2eb8336-dirty
(XEN) Processor: 410fd034: "ARM Limited", variant: 0x0, part 0xd03, rev 0x4
(XEN) 64-bit Execution:
(XEN) Processor Features: 0000000001002222 0000000000000000
(XEN) Exception Levels: EL3:64+32 EL2:64+32 EL1:64+32 EL0:64+32
(XEN) Extensions: FloatingPoint AdvancedSIMD GICv3-SysReg
(XEN) Debug Features: 0000000010305106 0000000000000000
(XEN) Auxiliary Features: 0000000000000000 0000000000000000
(XEN) Memory Model Features: 0000000000001122 0000000000000000
(XEN) ISA Features: 0000000000011120 0000000000000000
(XEN) 32-bit Execution:
(XEN) Processor Features: 00000131:10011011
(XEN) Instruction Sets: AArch32 A32 Thumb Thumb-2 Jazelle
(XEN) Extensions: GenericTimer Security
(XEN) Debug Features: 03010066
(XEN) Auxiliary Features: 00000000
(XEN) Memory Model Features: 10201105 40000000 01260000 02102211
(XEN) ISA Features: 02101110 13112111 21232042 01112131 00011142 00011121
(XEN) Generic Timer IRQ: phys=30 hyp=26 virt=27 Freq: 8000 KHz
(XEN) GICv3 initialization:
(XEN) gic_dist_addr=0x00000051a00000
(XEN) gic_maintenance_irq=25
(XEN) gic_rdist_stride=0
(XEN) gic_rdist_regions=1
(XEN) redistributor regions:
(XEN) - region 0: 0x00000051b00000 - 0x00000051bc0000
(XEN) GICv3 compatible with GICv2 cbase 0x00000052000000 vbase 0x00000052020000
(XEN) GICv3: 544 lines, (IID 0001143b).
(XEN) GICv3: CPU0: Found redistributor in region 0 @000000004002d000
(XEN) Using scheduler: SMP Credit Scheduler (credit)
(XEN) Allocated console ring of 16 KiB.
(XEN) Bringing up CPU1
(XEN) GICv3: CPU1: Found redistributor in region 0 @000000004004d000
(XEN) Bringing up CPU2
(XEN) GICv3: CPU2: Found redistributor in region 0 @000000004006d000
(XEN) Bringing up CPU3
(XEN) GICv3: CPU3: Found redistributor in region 0 @000000004008d000
(XEN) Bringing up CPU4
(XEN) GICv3: CPU4: Found redistributor in region 0 @00000000400ad000
(XEN) Bringing up CPU5
(XEN) GICv3: CPU5: Found redistributor in region 0 @00000000400cd000
(XEN) Brought up 6 CPUs
(XEN) P2M: 40-bit IPA with 40-bit PA and 8-bit VMID
(XEN) P2M: 3 levels with order-1 root, VTCR 0x80023558
(XEN) I/O virtualisation enabled
(XEN) - Dom0 mode: Relaxed
(XEN) Interrupt remapping enabled
(XEN) *** LOADING DOMAIN 0 ***
(XEN) Loading kernel from boot module @ 0000000085000000
(XEN) Allocating 1:1 mappings totalling 2048MB for dom0:
(XEN) BANK[0] 0x00000088000000-0x00000090000000 (128MB)
(XEN) BANK[1] 0x00000098000000-0x00000100000000 (1664MB)
(XEN) BANK[2] 0x00000960000000-0x00000970000000 (256MB)
(XEN) Grant table range: 0x0000097fe00000-0x0000097fe40000
(XEN) Ignore reserved memory reg, /reserved-memory/decoder_boot@0x84000000!
(XEN) Ignore reserved memory reg, /reserved-memory/encoder_boot@0x86000000!
(XEN) Ignore reserved memory reg, /reserved-memory/rpmsg@0x90000000!
(XEN) Ignore reserved memory reg, /reserved-memory/rpmsg_dma@0x90400000!
(XEN) Ignore reserved memory reg, /reserved-memory/decoder_rpc@0x92000000!
(XEN) Ignore reserved memory reg, /reserved-memory/encoder_rpc@0x92200000!
(XEN) Ignore reserved memory reg, /reserved-memory/dsp@0x92400000!
(XEN) Ignore reserved memory reg, /reserved-memory/encoder_reserved@0x94400000!
(XEN) Share gpio between Domains: /gpio@5d090000
(XEN) Share gpio between Domains: /gpio@5d0c0000
(XEN) HACK: skip /imx8_gpu_ss setup!
(XEN) NODE /m41_mem@0x94400000 conflicts with kernel address 0x00000088080000-0x0000008969a200
(XEN) Adjust load_offset to 0x00000008000000
(XEN) Allocating PPI 16 for event channel interrupt
(XEN) Loading zImage from 0000000085000000 to 0000000090080000-000000009169a200
(XEN)
(XEN) ****************************************
(XEN) Panic on CPU 0:
(XEN) Unable to copy the kernel in the hwdom memory
(XEN) ****************************************
(XEN)
(XEN) Reboot in five seconds...


U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (May 17 2019 - 00:08:15 +0000)

Can u give me some clues about this issue ? Like,  is it caused by uboot or scu firmware ?   The code is based on 4.14.98_2.0.0_ga+g87a19df release.

Regards,

-Minskey

7 Replies

6,797 Views
igorpadykov
NXP Employee
NXP Employee

Hi Minskey

for xen building and usage one can look at sect.5.6.11 Building Xen

attached Yocto Guide and sect.11.3 Xen Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

6,797 Views
minskey_guo
Contributor II

During Xen booting, Xen allocates 2048MB memory for Dom0 as follows:

(XEN) Allocating 1:1 mappings totalling 2048MB for dom0:
(XEN) BANK[0] 0x00000088000000-0x00000090000000 (128MB)
(XEN) BANK[1] 0x00000098000000-0x00000100000000 (1664MB)
(XEN) BANK[2] 0x00000960000000-0x00000970000000 (256MB)

And,  in mek-dom0.dts, m41 memory is 0x88800000 ~ 0x90000000(at the end of bandk[0]);

     m41_mem: m41_mem@0x94400000 {
             xen,passthrough;
             reg = <0 0x88800000 0 0x7800000>;
     };

The size of Dom0 kernel is 0x161A200,  and the size of m41_mem is 120MB/0x7800000B.  if we load dom0 kernel into bank0 (@0x88000000 + text_offset(0x8 00000),  there must be an overlapping with m41_mem. 

For my customized Mek Board,  when the conflict occurs,  Xen tries to load dom0 kernel to 0x90080000-0x9169a200, which is not in any bank allocated to Dom0.  So,  system panic when Xen tries to move Dom0 kernel from 0x92000000 to 0x9008000.

Can I change the memory range of m41_mem to other position, like bank1 ?  

Do I misunderstand anything ?

Regards,

-minskey

0 Kudos
Reply

6,797 Views
igorpadykov
NXP Employee
NXP Employee

Hi minskey

partition and memory management are performed by scfw, so one can look at its documentation:

SCFW Porting Kit


Best regards
igor

0 Kudos
Reply

6,797 Views
minskey_guo
Contributor II

Yes, I read the scfw doc.   What I want to understand is :

  

    The memory of Bank0 allocated to Dom0 is only 128M,  but the m41_memory occupies 120M,  only 8M for Dom0 kernel, although the size of Dom0 kernel is 0x161A200.  

     I tried to move m41-mem to 0x98800000, it does work. But I don't know if there is any potential issue here.

thanks,

-minskey

0 Kudos
Reply

6,797 Views
minskey_guo
Contributor II

At last, I found the root cause.   In uboot config file (imx8qm_mek_defconfig),  it reserves that range of memory for CM41, but my friend remove the configuration.  Add it back fix this issue,

CONFIG_BOOTAUX_RESERVED_MEM_BASE=0x88000000
CONFIG_BOOTAUX_RESERVED_MEM_SIZE=0x08000000

0 Kudos
Reply

6,797 Views
minskey_guo
Contributor II

Now, I move the kernel Image load address from 0x85000000 to 0x92000000 as qm MEK board, Xen boot makes some progress.  But still panic in uboot kernel_zimage_load(). 

Do we have a document  which lists the memory layout for Xen, Dom0, Domu, M4_0/1 ?

The following is the Xen message during booting.

 Xen 4.11.1-pre
(XEN) Xen version 4.11.1-pre (minskey@) (aarch64-poky-linux-gcc (GCC) 7.3.0) debug=n Sun May 26 22:13:12 UTC 2019
(XEN) Latest ChangeSet: Tue Apr 16 16:24:07 2019 +0800 git:2eb8336-dirty
(XEN) Processor: 410fd034: "ARM Limited", variant: 0x0, part 0xd03, rev 0x4
(XEN) 64-bit Execution:
(XEN) Processor Features: 0000000001002222 0000000000000000
(XEN) Exception Levels: EL3:64+32 EL2:64+32 EL1:64+32 EL0:64+32
(XEN) Extensions: FloatingPoint AdvancedSIMD GICv3-SysReg
(XEN) Debug Features: 0000000010305106 0000000000000000
(XEN) Auxiliary Features: 0000000000000000 0000000000000000
(XEN) Memory Model Features: 0000000000001122 0000000000000000
(XEN) ISA Features: 0000000000011120 0000000000000000
(XEN) 32-bit Execution:
(XEN) Processor Features: 00000131:10011011
(XEN) Instruction Sets: AArch32 A32 Thumb Thumb-2 Jazelle
(XEN) Extensions: GenericTimer Security
(XEN) Debug Features: 03010066
(XEN) Auxiliary Features: 00000000
(XEN) Memory Model Features: 10201105 40000000 01260000 02102211
(XEN) ISA Features: 02101110 13112111 21232042 01112131 00011142 00011121
(XEN) Generic Timer IRQ: phys=30 hyp=26 virt=27 Freq: 8000 KHz
(XEN) GICv3 initialization:
(XEN) gic_dist_addr=0x00000051a00000
(XEN) gic_maintenance_irq=25
(XEN) gic_rdist_stride=0
(XEN) gic_rdist_regions=1
(XEN) redistributor regions:
(XEN) - region 0: 0x00000051b00000 - 0x00000051bc0000
(XEN) GICv3 compatible with GICv2 cbase 0x00000052000000 vbase 0x00000052020000
(XEN) GICv3: 544 lines, (IID 0001143b).
(XEN) GICv3: CPU0: Found redistributor in region 0 @000000004002d000
(XEN) Using scheduler: SMP Credit Scheduler (credit)
(XEN) Allocated console ring of 16 KiB.
(XEN) Bringing up CPU1
(XEN) GICv3: CPU1: Found redistributor in region 0 @000000004004d000
(XEN) Bringing up CPU2
(XEN) GICv3: CPU2: Found redistributor in region 0 @000000004006d000
(XEN) Bringing up CPU3
(XEN) GICv3: CPU3: Found redistributor in region 0 @000000004008d000
(XEN) Bringing up CPU4
(XEN) GICv3: CPU4: Found redistributor in region 0 @00000000400ad000
(XEN) Bringing up CPU5
(XEN) GICv3: CPU5: Found redistributor in region 0 @00000000400cd000
(XEN) Brought up 6 CPUs
(XEN) P2M: 40-bit IPA with 40-bit PA and 8-bit VMID
(XEN) P2M: 3 levels with order-1 root, VTCR 0x80023558
(XEN) I/O virtualisation enabled
(XEN) - Dom0 mode: Relaxed
(XEN) Interrupt remapping enabled
(XEN) *** LOADING DOMAIN 0 ***
(XEN) Loading kernel from boot module @ 0000000092000000
(XEN) Allocating 1:1 mappings totalling 2048MB for dom0:
(XEN) BANK[0] 0x00000088000000-0x00000090000000 (128MB)
(XEN) BANK[1] 0x00000098000000-0x00000100000000 (1664MB)
(XEN) BANK[2] 0x00000960000000-0x00000970000000 (256MB)
(XEN) Grant table range: 0x0000097fe00000-0x0000097fe40000
(XEN) Ignore reserved memory reg, /reserved-memory/decoder_boot@0x84000000!
(XEN) Ignore reserved memory reg, /reserved-memory/encoder_boot@0x86000000!
(XEN) Ignore reserved memory reg, /reserved-memory/rpmsg@0x90000000!
(XEN) Ignore reserved memory reg, /reserved-memory/rpmsg_dma@0x90400000!
(XEN) Ignore reserved memory reg, /reserved-memory/decoder_rpc@0x92000000!
(XEN) Ignore reserved memory reg, /reserved-memory/encoder_rpc@0x92200000!
(XEN) Ignore reserved memory reg, /reserved-memory/dsp@0x92400000!
(XEN) Ignore reserved memory reg, /reserved-memory/encoder_reserved@0x94400000!
(XEN) Share gpio between Domains: /gpio@5d090000
(XEN) Share gpio between Domains: /gpio@5d0c0000
(XEN) HACK: skip /imx8_gpu_ss setup!
(XEN) NODE /m41_mem@0x94400000 conflicts with kernel address 0x00000088080000-0x0000008969a200
(XEN) Adjust load_offset to 0x00000008000000
(XEN) Allocating PPI 16 for event channel interrupt
(XEN) Loading zImage from 0000000092000000 to 0000000090080000-000000009169a200
(XEN)
(XEN) ****************************************
(XEN) Panic on CPU 0:
(XEN) Unable to copy the kernel in the hwdom memory
(XEN) ****************************************
(XEN)
(XEN) Reboot in five seconds...
 

thanks,

-minskey

0 Kudos
Reply

4,275 Views
azkaaa
Contributor I

Hello! I know it's been a while since the issue happened. But I would like to ask if there is any latest update on how to resolve the issue?

However, I found a similar issue using a different board from apalis imx8qm ixora carrier board.

Can someone please explain the continuation of this issue?

This is my full boot message

Xen 4.18.3
(XEN) Xen version 4.18.3 (create01@) (aarch64-tdx-linux-gcc (GCC) 13.3.0) debug=n Thu Sep 19 12:54:22 WIB 2024
(XEN) Latest ChangeSet: Wed Aug 14 17:49:51 2024 -0700 git:781c251261
(XEN) build-id: 095d17573dab5de30cb0f1fb3674dfe9ca0fb235
(XEN) Console output is synchronous.
(XEN) Processor: 00000000410fd034: "ARM Limited", variant: 0x0, part 0xd03,rev 0x4
(XEN) 64-bit Execution:
(XEN) Processor Features: 0000000001002222 0000000000000000
(XEN) Exception Levels: EL3:64+32 EL2:64+32 EL1:64+32 EL0:64+32
(XEN) Extensions: FloatingPoint AdvancedSIMD GICv3-SysReg
(XEN) Debug Features: 0000000010305106 0000000000000000
(XEN) Auxiliary Features: 0000000000000000 0000000000000000
(XEN) Memory Model Features: 0000000000001122 0000000000000000
(XEN) ISA Features: 0000000000011120 0000000000000000
(XEN) 32-bit Execution:
(XEN) Processor Features: 0000000000000131:0000000010011011
(XEN) Instruction Sets: AArch32 A32 Thumb Thumb-2 Jazelle
(XEN) Extensions: GenericTimer Security
(XEN) Debug Features: 0000000003010066
(XEN) Auxiliary Features: 0000000000000000
(XEN) Memory Model Features: 0000000010201105 0000000040000000
(XEN) 0000000001260000 0000000002102211
(XEN) ISA Features: 0000000002101110 0000000013112111 0000000021232042
(XEN) 0000000001112131 0000000000011142 0000000000011121
(XEN) Using SMC Calling Convention v1.4
(XEN) Using PSCI v1.1
(XEN) SMP: Allowing 6 CPUs
(XEN) Generic Timer IRQ: phys=30 hyp=26 virt=27 Freq: 8000 KHz
(XEN) GICv3 initialization:
(XEN) gic_dist_addr=0x00000051a00000
(XEN) gic_maintenance_irq=25
(XEN) gic_rdist_stride=0
(XEN) gic_rdist_regions=1
(XEN) redistributor regions:
(XEN) - region 0: 0x00000051b00000 - 0x00000051bc0000
(XEN) GICv3 compatible with GICv2 cbase 0x00000052000000 vbase 0x00000052020000
(XEN) GICv3: 544 lines, (IID 0001143b).
(XEN) GICv3: CPU0: Found redistributor in region 0 @000002004001c000
(XEN) XSM Framework v1.0.1 initialized
(XEN) Initialising XSM SILO mode
(XEN) Could not find scheduler: null
(XEN) Using 'SMP Credit Scheduler rev2' (credit2)
(XEN) Using scheduler: SMP Credit Scheduler rev2 (credit2)
(XEN) Initializing Credit2 scheduler
(XEN) load_precision_shift: 18
(XEN) load_window_shift: 30
(XEN) underload_balance_tolerance: 0
(XEN) overload_balance_tolerance: -3
(XEN) runqueues arrangement: socket
(XEN) cap enforcement granularity: 10ms
(XEN) load tracking window length 1073741824 ns
(XEN) Allocated console ring of 64 KiB.
(XEN) CPU0: Guest atomics will try 13 times before pausing the domain
(XEN) Bringing up CPU1
(XEN) GICv3: CPU1: Found redistributor in region 0 @000002004003c000
(XEN) CPU1: Guest atomics will try 14 times before pausing the domain
(XEN) CPU 1 booted.
(XEN) Bringing up CPU2
(XEN) GICv3: CPU2: Found redistributor in region 0 @000002004005c000
(XEN) CPU2: Guest atomics will try 14 times before pausing the domain
(XEN) CPU 2 booted.
(XEN) Bringing up CPU3
(XEN) GICv3: CPU3: Found redistributor in region 0 @000002004007c000
(XEN) CPU3: Guest atomics will try 15 times before pausing the domain
(XEN) CPU 3 booted.
(XEN) Bringing up CPU4
(XEN) CPU4 MIDR (0x00000000410fd082) does not match boot CPU MIDR (0x00000000410fd034),
(XEN) disable cpu (see big.LITTLE.txt under docs/).
(XEN) CPU4 never came online
(XEN) Failed to bring up CPU 4 (error -5)
(XEN) Bringing up CPU5
(XEN) CPU5 MIDR (0x00000000410fd082) does not match boot CPU MIDR (0x00000000410fd034),
(XEN) disable cpu (see big.LITTLE.txt under docs/).
(XEN) CPU5 never came online
(XEN) Failed to bring up CPU 5 (error -5)
(XEN) Brought up 4 CPUs
(XEN) smmu: /iommu@51400000: probing hardware configuration...
(XEN) smmu: /iommu@51400000: SMMUv2 with:
(XEN) smmu: /iommu@51400000: stage 2 translation
(XEN) smmu: /iommu@51400000: stream matching with 32 register groups, mask 0x7fbf<2>smmu: /iommu@51400000: 32 context banks (0 stage-2 only)
(XEN) smmu: /iommu@51400000: Stage-2: 48-bit IPA -> 48-bit PA
(XEN) smmu: /iommu@51400000: registered 0 master devices
(XEN) I/O virtualisation enabled
(XEN) - Dom0 mode: Relaxed
(XEN) P2M: 40-bit IPA with 40-bit PA and 8-bit VMID
(XEN) P2M: 3 levels with order-1 root, VTCR 0x0000000080023558
(XEN) Scheduling granularity: cpu, 1 CPU per sched-resource
(XEN) Initializing Credit2 scheduler
(XEN) load_precision_shift: 18
(XEN) load_window_shift: 30
(XEN) underload_balance_tolerance: 0
(XEN) overload_balance_tolerance: -3
(XEN) runqueues arrangement: socket
(XEN) cap enforcement granularity: 10ms
(XEN) load tracking window length 1073741824 ns
(XEN) Logical CPU 0 in Pool-0 (Scheduler id: -1).
(XEN) Adding cpu 0 to runqueue 0
(XEN) First cpu on runqueue, activating
(XEN) Logical CPU 1 in Pool-0 (Scheduler id: -1).
(XEN) Adding cpu 1 to runqueue 0
(XEN) Logical CPU 2 in Pool-0 (Scheduler id: -1).
(XEN) Adding cpu 2 to runqueue 0
(XEN) Logical CPU 3 in Pool-0 (Scheduler id: -1).
(XEN) Adding cpu 3 to runqueue 0
(XEN) alternatives: Patching with alt table 00000200002cdad0 -> 00000200002cecb8
(XEN) *** LOADING DOMAIN 0 ***
(XEN) Loading d0 kernel from boot module @ 0000000880400000
(XEN) Loading ramdisk from boot module @ 0000000882000000
(XEN) Allocating 1:1 mappings totalling 2048MB for dom0:
(XEN) BANK[0] 0x00000098000000-0x00000100000000 (1664MB)
(XEN) BANK[1] 0x00000898000000-0x000008a0000000 (128MB)
(XEN) BANK[2] 0x000009e0000000-0x000009f0000000 (256MB)
(XEN) Grant table range: 0x0000088b600000-0x0000088b640000
(XEN) Allocating PPI 16 for event channel interrupt
(XEN) d0: extended region 0: 0x18000000->0x2be00000
(XEN) d0: extended region 1: 0x31a00000->0x3b200000
(XEN) d0: extended region 2: 0x3b800000->0x51200000
(XEN) d0: extended region 3: 0x100000000->0x87fe00000
(XEN) d0: extended region 4: 0xa00000000->0xffffe00000
(XEN) Loading zImage from 0000000880400000 to 0000000098000000-0000000099b20000
(XEN)
(XEN) ****************************************
(XEN) Panic on CPU 0:
(XEN) Unable to copy the kernel in the hwdom memory
(XEN) ****************************************
(XEN)
(XEN) Reboot in five seconds...

 

thanks
-Azkaaa

0 Kudos
Reply