imx8qm IBIS model error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qm IBIS model error

2,738件の閲覧回数
JavierJimenez
Contributor I

Hello,

I was trying to simulate IBIS model imx8qm but it gives me errors (see picture).

Do you have an alternative IBIS model for simulation?

 

Kind regards,

Javier

 

 

0 件の賞賛
返信
3 返答(返信)

2,732件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

In the following link, you will find the latest IBIS model available: https://www.nxp.com/downloads/en/ibis-model/IMX8QM-IBIS.zip 

 

May I ask if this is the one you are working with?

 

BR,

Ivan.

0 件の賞賛
返信

2,724件の閲覧回数
JavierJimenez
Contributor I

Yes, is the same file that I was working with and it seems that it contains errors.

 

Kind regards,

Javi

0 件の賞賛
返信

2,720件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

Thank you for confirming this.

 

I have checked and there is already a case in progress for this petition that is still open. So please continue the support through salesforce, the internal team is already working on this.

 

Have a nice day!

 

BR,

Ivan.

 

 

0 件の賞賛
返信