imx8mq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq

1,129 Views
srinu_inaganti
Contributor III

Hi Team,

Any one help me how to enable extended USB 2.0 ports via

USB => USBUSB2513BI(Hub controller) to Three USB lines

How to achieve ? is there any DTS file changes required ?

Regards,

Srinu I

0 Kudos
Reply
1 Reply

1,054 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinu

example dts file with hub can be found in imx8mq-nitrogen8m.dts

linux-imx6/imx8mq-nitrogen8m.dts at boundary-imx_4.19.x_1.1.0-pass2 · boundarydevices/linux-imx6 · G... 

use only USB 2.0 signal pins, USB3.0 signals pins can be left unconnected.

pastedImage_2.jpg

pastedImage_3.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply