imx8mq u-boot acessing LED

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mq u-boot acessing LED

2,836件の閲覧回数
mark-calaway
Contributor II

I apply patch for SPI and its enable in u-boot, while giving command in u-boot > help its showing sspi and its enabled. but i need a command line for blinking LED , i try u-boot=> sspi 0:2.0 32 A
00000000
u-boot=> sspi 0:2.0 32 B
00000000
u-boot=> sspi 0:2.0 32 0
00000000
u-boot=> sspi 0:2.0 32 F
00000000  and i get this 00000000

i have one doubt only is there any led blinking or glowing process in sspi via gpio pins is it possible or what? and how its glow using command line or will anyone provided me a proper patch file for imx8mq source code for u-boot version U-Boot SPL 2020.04-5.4.70-2.3.2+g185bdaaaf5  and Linux version Linux version 5.4.70-2.3.2+ (oe-user@oe-host) (gcc version 9.2.0 (GCC)) .

I attached the patch file which i apply in my build so please take a look on it.

Thanks in  advance.

タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,758件の閲覧回数
_angelo_
Contributor III

Sorry, cannot do the job for you, i don't know your schematic. GPIO from userspace, if gpios are free, does not need any patch, should work quite well.

1) check your spi<->pgio converter is detected and gpios are available from userspace, seems yes

2) access them by export, supposing your led is connected to gpio24, by

echo 24 > /sys/class/gpio/export
echo out > /sys/class/gpio24/direction
echo 1 > /sys/class/gpio24/value
echo 0 > /sys/class/gpio24/value

0 件の賞賛
返信

2,777件の閲覧回数
_angelo_
Contributor III

Please provide the spi -> gpio chip you are using. You can initialize it and send commands in a loop to have the led blinking.

0 件の賞賛
返信

2,772件の閲覧回数
mark-calaway
Contributor II

thanks for the reply,

is there any specific patch file for this board(IMX8MQ) to access LED via spi or check whether i send you a patch file,that is correct one or not? 

this is the print i get for spi and gpio.

(LED) 2023.10.13-05:54:40.811 <INFO> [LED_Init : 700] SPI-INFO : Mode(3), Bits/Word(8), Speed(10000 kHz)
(LED) 2023.10.13-05:54:40.811 <INFO> [LED_Init : 705] LED_Init_4
(GPIO) 2023.10.13-05:54:40.811 <INFO> [GPIO_Export : 118] /sys/class/gpio/export for GPIO[132]
(GPIO) 2023.10.13-05:54:40.811 <INFO> [GPIO_Export : 118] /sys/class/gpio/export for GPIO[125]
(GPIO) 2023.10.13-05:54:40.811 <INFO> [GPIO_Export : 118] /sys/class/gpio/export for GPIO[126]
(GPIO) 2023.10.13-05:54:40.811 <INFO> [GPIO_Export : 118] /sys/class/gpio/export for GPIO[11]

please verify the patchfile i provide.  thanks in advance.

 

0 件の賞賛
返信

2,756件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

(y)

0 件の賞賛
返信