imx8mq qt5 zxdg_shell_v6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq qt5 zxdg_shell_v6

1,267 Views
kangmw086
Contributor III

hi.

use info.

imx8mq, yocto rocko,  linux imx8mqevk 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d.

qt5.9.4 used.

When you run qt5 application, it works fine.

However, the value of the qt application's combox is not selected.

If you click on combox and select another area, the application dies with the following error:

zxdg_shell_v6@19: error 2: xdg_popup was not created on the topmost popup
The Wayland connection experienced a fatal error (Protocol error)

 

Is it solvable?

Tags (1)
0 Kudos
Reply
1 Reply

1,263 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello kangmw086,

 

This is a bug in qt appears to be fixed in most recent QT

https://bugreports.qt.io/browse/QTBUG-81952

Please update your yocto with latest version.

 

Regards

 

 

0 Kudos
Reply