Frame rate support in I.MX8M MINI processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Frame rate support in I.MX8M MINI processor

1,399 Views
viralvasa
Contributor I

We are using I.MX8M MINI processor's MIPI DSI Interface. We are using single lane to connect it to our display LCD. Video that needs to be displayed is of resolution 960x320 pixel ( we are using RGB 565/666 mode)

Datasheet mentions 1080p@60fps.

Can we achieve Frame rate of 120 fps with this resolution ? 

0 Kudos
Reply
1 Reply

1,387 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello viralvasa,

If the current MIPI driver custom resolution or support that resolution with your driver, yes its possible to get 120fps.

 

regards

 

0 Kudos
Reply