imx8mq custom board android cannot boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mq custom board android cannot boot

ソリューションへジャンプ
10,877件の閲覧回数
pyh0603
Contributor III

Hello,

Release: android_p11.0.0_2.6.0

Board: i.MX8MQ based custom board

 

Linux kernel software modification:

  1. Closing pcie1 & pcie2 in Linux device tree

 

The main differences between our customized imx8mq and the hardware of the development board are as follows:

1. CSI, camera interface, not used, grounded in design,

2. Sdio1, the hinge type microSD peripheral is deleted, and only EMMC flash is connected,

3. The audio codec chip connected to sai2 is different,

4. PCIe, the first PCIe is connected to WiFi / BT module, the module cannot be purchased temporarily, and the WiFi / BT module is suspended.

5. PCIe. The second PCIe is not used and is suspended.

6. All four UART serial ports are used, and uart4 of the development board is used as GPIO;

7. More peripherals connected to I2C;

8. SPI interface is connected to MCU; The development board is used as GPIO;

9. USB type-C CC chip replacement;

10. GPIO of CPU is used as the control signal of peripheral circuit

 

Partial log:

[ 76.568750][ T367] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400000 fc=4000000 cc=32 chg=a
[ 77.438135][ T366] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0
[ 77.473417][ T366] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0
[ 77.511485][ T366] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0
[ 77.525500][ T223] type=1107 audit(84.895:5): uid=0 auid=4294967295 ses=4294967295 subj=u:r:init:s0 msg='avc: denied { set } for property=vendor.display.state pid=366 uid=1000 gid=1003 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=property_service permissive=0'
[ 78.027522][ T501] read descriptors
[ 78.031776][ T501] read strings
[ 78.285273][ T35] usb 1-1: new high-speed USB device number 2 using dummy_hcd
[ 78.297485][ T140] android_work: sent uevent USB_STATE=CONNECTED
[ 78.545683][ T35] usb 1-1: Dual-Role OTG device on HNP port
[ 78.561264][ T35] usb 1-1: New USB device found, idVendor=18d1, idProduct=4ee7, bcdDevice= 4.40
[ 78.570460][ T35] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 78.578496][ T35] usb 1-1: Product: EVK_8MQ
[ 78.583033][ T35] usb 1-1: Manufacturer: nxp
[ 78.587692][ T35] usb 1-1: SerialNumber: 0c2119d6f6c99ecb
[ 78.601754][ T140] android_work: sent uevent USB_STATE=CONFIGURED
[ 78.605154][ T1] init: starting service 'bootanim'...
[ 78.617138][ T1] init: Control message: Processed ctl.start for 'bootanim' from pid: 382 (/system/bin/surfaceflinger)
[ 84.676401][ T223] type=1400 audit(92.047:6): avc: denied { read } for comm="Binder:231_2" name="wakeup6" dev="sysfs" ino=32038 scontext=u:r:system_suspend:s0 tcontext=u:object_r:sysfs:s0 tclass=dir permissive=0
[ 85.504301][ T334] AidlLazyServiceRegistrar: Process has 1 (of 1 available) client(s) in use after notification android.apex.IApexService has clients: 1

[ 115.305036][ T1] init: Untracked pid 600 exited with status 0
[ 115.311353][ T1] init: Untracked pid 602 exited with status 0
[ 115.455317][ T1] init: Untracked pid 607 exited with status 0
[ 115.461746][ T1] init: Untracked pid 609 exited with status 0
[ 115.557242][ T1] init: Untracked pid 613 exited with status 0
[ 115.563505][ T1] init: Untracked pid 615 exited with status 0
[ 115.648026][ T1] init: Untracked pid 619 exited with status 0
[ 115.654351][ T1] init: Untracked pid 621 exited with status 0
[ 115.779646][ T1] init: Untracked pid 625 exited with status 0
[ 115.785939][ T1] init: Untracked pid 627 exited with status 0
[ 136.570468][ T367] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400000 fc=4000000 cc=32 chg=a
[ 149.855622][ T1] init: Untracked pid 699 exited with status 0
[ 149.861916][ T1] init: Untracked pid 701 exited with status 0
[ 149.990122][ T1] init: Untracked pid 705 exited with status 0
[ 149.996379][ T1] init: Untracked pid 707 exited with status 0
[ 150.082135][ T1] init: Untracked pid 711 exited with status 0
[ 150.088406][ T1] init: Untracked pid 713 exited with status 0
[ 150.186779][ T1] init: Untracked pid 716 exited with status 0
[ 150.194170][ T1] init: Untracked pid 718 exited with status 0
[ 150.323796][ T1] init: Untracked pid 722 exited with status 0
[ 150.331215][ T1] init: Untracked pid 724 exited with status 0
[ 157.823705][ T577] sysrq: Show Blocked State
[ 157.832432][ T577] sysrq: Show backtrace of all active CPUs
[ 157.838611][ C1] sysrq: CPU1:
[ 157.841872][ C1] Call trace:
[ 157.845156][ C1] dump_backtrace+0x0/0x1d0
[ 157.849570][ C1] show_stack+0x1c/0x2c
[ 157.853646][ C1] showacpu+0x7c/0x8c
[ 157.857547][ C1] flush_smp_call_function_queue+0x174/0x250
[ 157.863404][ C1] generic_smp_call_function_single_interrupt+0x18/0x28
[ 157.870247][ C1] ipi_handler+0x8c/0x114
[ 157.874476][ C1] handle_percpu_devid_fasteoi_ipi+0x7c/0x19c
[ 157.880415][ C1] __handle_domain_irq+0x80/0xd0
[ 157.885366][ C1] gic_handle_irq+0x6c/0x124
[ 157.889869][ C1] el1_irq+0xe4/0x1c0
[ 157.893754][ C1] cpuidle_enter_state+0x1c4/0x52c
[ 157.898735][ C1] cpuidle_enter+0x3c/0x58
[ 157.903046][ C1] do_idle+0x1e0/0x298
[ 157.906984][ C1] cpu_startup_entry+0x28/0x2c
[ 157.911629][ C1] secondary_start_kernel+0x1ac/0x1e4
[ 157.916998][ C3] sysrq: CPU3:
[ 157.920368][ C3] Call trace:
[ 157.923565][ C3] dump_backtrace+0x0/0x1d0
[ 157.927939][ C3] show_stack+0x1c/0x2c
[ 157.931974][ C3] showacpu+0x7c/0x8c
[ 157.935844][ C3] flush_smp_call_function_queue+0x174/0x250
[ 157.941691][ C3] generic_smp_call_function_single_interrupt+0x18/0x28
[ 157.948500][ C3] ipi_handler+0x8c/0x114
[ 157.952706][ C3] handle_percpu_devid_fasteoi_ipi+0x7c/0x19c
[ 157.958639][ C3] __handle_domain_irq+0x80/0xd0
[ 157.963454][ C3] gic_handle_irq+0x6c/0x124
[ 157.967913][ C3] el1_irq+0xe4/0x1c0
[ 157.971772][ C3] cpuidle_enter_state+0x1c4/0x52c
[ 157.976752][ C3] cpuidle_enter+0x3c/0x58
[ 157.981042][ C3] do_idle+0x1e0/0x298
[ 157.984977][ C3] cpu_startup_entry+0x28/0x2c
[ 157.989614][ C3] secondary_start_kernel+0x1ac/0x1e4
[ 158.332845][ T35] binder: release 535:574 transaction 3300 out, still active
[ 158.340863][ T35] binder: undelivered TRANSACTION_COMPLETE
[ 158.552975][ T1] init: Service 'zygote' (pid 352) received signal 9
[ 158.560111][ T1] init: Sending signal 9 to service 'zygote' (pid 352) process group...
[ 158.572058][ T1] libprocessgroup: Successfully killed process cgroup uid 0 pid 352 in 1ms
[ 158.585921][ T1] init: starting service 'exec 15 (/system/bin/vdc volume abort_fuse)'...
[ 158.622236][ T1] init: Command 'write /sys/power/state on' action=onrestart (<Service 'zygote' onrestart>:2) took 7ms and failed: Unable to write to file '/sys/power/state': Unable to write file contents: Invalid argument
[ 158.643690][ T1] init: Sending signal 9 to service 'audioserver' (pid 376) process group...
[ 158.720464][ T1] libprocessgroup: Successfully killed process cgroup uid 1041 pid 376 in 66ms
[ 158.735541][ T1] init: Command 'restart audioserver' action=onrestart (<Service 'zygote' onrestart>:3) took 92ms and succeeded
[ 158.747616][ T1] init: Sending signal 9 to service 'cameraserver' (pid 438) process group...
[ 158.799542][ T1] libprocessgroup: Successfully killed process cgroup uid 1047 pid 438 in 41ms
[ 160.503942][ T334] AidlLazyServiceRegistrar: Process has 0 (of 1 available) client(s) in use after notification android.apex.IApexService has clients: 0
[ 160.518527][ T334] AidlLazyServiceRegistrar: Shutdown prevented by forcePersist override flag.
[ 164.556167][ T223] type=1400 audit(171.926:7): avc: denied { read } for comm="Binder:231_1" name="wakeup6" dev="sysfs" ino=32038 scontext=u:r:system_suspend:s0 tcontext=u:object_r:sysfs:s0 tclass=dir permissive=0
[ 165.504797][ T334] AidlLazyServiceRegistrar: Process has 1 (of 1 available) client(s) in use after notification android.apex.IApexService has clients: 1
[ 170.504728][ T334] AidlLazyServiceRegistrar: Process has 0 (of 1 available) client(s) in use after notification android.apex.IApexService has clients: 0
[ 170.518577][ T334] AidlLazyServiceRegistrar: Shutdown prevented by forcePersist override flag.

 

Current problems

  1. The Linux kernel starts normally and has entered the file system normally, but cannot enter the Android system
  2. According to the startup log Why does the zygote process always restart regularly

 

I have attached the startup log of the custom imx8mq board and the log of imx8mq-evk board

 

Thandks!

Look forward to your reply!

ラベル(1)
0 件の賞賛
返信
1 解決策
10,731件の閲覧回数
pyh0603
Contributor III

Thank you for your reply.

I have solved the problem that the imx8mq custom board cannot enter the boot animation.

 

It may be that there is a voltage drop in the GPU power supply voltage of our customized board, resulting in the abnormal operation of the GPU. If I set the operating voltage VDD_GPU_0V9 of GPU from 0.9V to 1.1V in uboot, Android can enter the boot animation normally

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
10,732件の閲覧回数
pyh0603
Contributor III

Thank you for your reply.

I have solved the problem that the imx8mq custom board cannot enter the boot animation.

 

It may be that there is a voltage drop in the GPU power supply voltage of our customized board, resulting in the abnormal operation of the GPU. If I set the operating voltage VDD_GPU_0V9 of GPU from 0.9V to 1.1V in uboot, Android can enter the boot animation normally

0 件の賞賛
返信
10,846件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you also attach the  logcat msg?

0 件の賞賛
返信
10,822件の閲覧回数
pyh0603
Contributor III

 

I copied the error log as follows, and put all the logs in the attachment.

Please help analyze it, thank you

130|evk_8mq:/ $
130|evk_8mq:/ $
130|evk_8mq:/ $
130|evk_8mq:/ $ logcat *:E
[ 503.572186][ T205] logd: logdr: UID=2000 GID=2000 PID=2736 b tail=0 logMask=99 pid=0 start=0ns timeout=0ns
--------- beginning of kernel
01-01 00:00:02.163 0 0 E [ T1] Warning: unable to open an initial console.
01-01 00:00:02.270 0 0 E [ T1] init: alias lines in modules.alias must have 3 entries, not 4
01-01 00:00:02.275 0 0 E [ T1] init: alias lines in modules.alias must have 3 entries, not 4
01-01 00:00:02.725 0 0 E : [ T1] trusty trusty: failed to get version: -1
01-01 00:00:02.947 0 0 E : [ T126] phy phy-381f0040.usb-phy.1: failed to get power supply
01-01 00:00:02.954 0 0 E : [ T126] phy phy-381f0040.usb-phy.1: failed to get power supply
01-01 00:00:03.051 0 0 E : [ T1] trusty-virtio trusty:trusty-virtio: trusty_load_device_descr: virtio get descr returned (-1)
01-01 00:00:03.061 0 0 E : [ T1] trusty-virtio trusty:trusty-virtio: failed (-19) to load device descr
01-01 00:00:03.070 0 0 E : [ T1] trusty-virtio trusty:trusty-virtio: Failed to add virtio devices
01-01 00:00:04.436 0 0 E [ T1] cgroup: Unknown subsys name 'schedtune'
01-01 00:00:05.208 0 0 F [ T190] wlan: Loading MWLAN driver
01-01 00:00:05.214 0 0 F [ T190] wlan: Driver loaded successfully
01-01 00:00:05.214 0 0 F [ T109] wlan: Register to Bus Driver...
01-01 00:00:05.224 0 0 F [ T109] wlan: Register to Bus Driver Done
01-01 00:00:05.550 0 0 E : [ T190] ak4458 2-0010: Failed to set acks: -11
01-01 00:00:05.590 0 0 E : [ T190] ak4458 2-0012: Failed to set acks: -11
01-01 00:00:05.639 0 0 E : [ T190] ak4458 2-0011: Failed to set acks: -11
01-01 00:00:05.681 0 0 E [ T190] debugfs: File 'Playback' in directory 'dapm' already present!
01-01 00:00:05.689 0 0 E [ T190] debugfs: File 'Capture' in directory 'dapm' already present!
01-01 00:00:05.722 0 0 E : [ T190] snvs_rtc 30370000.snvs:snvs-rtc-lp: snvs rtc: trusty snvs driver failed to probe! nr=0xb5000000 ret=-1. Use normal mode.
01-01 00:00:33.431 0 0 E [ T1] init: /dev/block/by-name/userdata is not dm device: No such file or directory
01-01 00:00:33.462 0 0 E [ T1] init: [libfs_mgr]mount_with_alternatives(): skipping mount due to invalid magic, mountpoint=/data blk_dev=/dev/block/dm-4 rec[1].fs_type=ext4
01-01 00:00:58.691 0 0 E [ T297] apexd: Can't open /system_ext/apex for reading : No such file or directory
01-01 00:00:58.699 0 0 E [ T297] apexd: Can't open /product/apex for reading : No such file or directory
01-01 00:00:58.708 0 0 E [ T297] apexd: Can't open /vendor/apex for reading : No such file or directory
--------- beginning of main
--------- beginning of system
03-03 02:54:29.355 495 495 E HistoricalRegistry: Interaction before persistence initialized
03-03 02:54:29.360 495 495 E HistoricalRegistry: Interaction before persistence initialized
03-03 02:54:29.377 495 495 E DisplayPowerController: failed to set up display white-balance: java.lang.IllegalStateException: cannot find light sensor
03-03 02:54:29.401 217 223 E android.system.suspend@1.0-service: Error opening kernel wakelock stats for: wakeup5: Permission denied
03-03 02:54:29.693 495 495 E DefaultPermGrantPolicy: Permission not found: com.google.android.googleapps.permission.GOOGLE_AUTH
03-03 02:54:29.693 495 495 E DefaultPermGrantPolicy: Permission not found: com.android.launcher.permission.READ_SETTINGS
03-03 02:54:29.693 495 495 E DefaultPermGrantPolicy: Permission not found: com.android.launcher.permission.WRITE_SETTINGS
03-03 02:54:29.695 495 495 E DefaultPermGrantPolicy: Permission not found: com.android.smspush.WAPPUSH_MANAGER_BIND
03-03 02:54:29.696 495 495 E DefaultPermGrantPolicy: Permission not found: android.permission.MANAGE_WIFI_WHEN_WIRELESS_CONSENT_REQUIRED
03-03 02:54:29.699 495 495 E DefaultPermGrantPolicy: Permission not found: android.car.permission.CONTROL_CAR_CLIMATE
03-03 02:54:29.699 495 495 E DefaultPermGrantPolicy: Permission not found: android.car.permission.CAR_CONTROL_AUDIO_VOLUME
03-03 02:54:29.702 495 495 E DefaultPermGrantPolicy: Permission not found: com.sec.android.provider.badge.permission.READ
03-03 02:54:29.702 495 495 E DefaultPermGrantPolicy: Permission not found: com.sec.android.provider.badge.permission.WRITE
03-03 02:54:29.702 495 495 E DefaultPermGrantPolicy: Permission not found: com.htc.launcher.permission.READ_SETTINGS
03-03 02:54:29.702 495 495 E DefaultPermGrantPolicy: Permission not found: com.htc.launcher.permission.UPDATE_SHORTCUT
03-03 02:54:29.702 495 495 E DefaultPermGrantPolicy: Permission not found: com.sonyericsson.home.permission.BROADCAST_BADGE
03-03 02:54:29.702 495 495 E DefaultPermGrantPolicy: Permission not found: com.sonymobile.home.permission.PROVIDER_INSERT_BADGE
03-03 02:54:29.704 495 495 E DefaultPermGrantPolicy: Permission not found: com.anddoes.launcher.permission.UPDATE_COUNT
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: com.majeur.launcher.permission.UPDATE_BADGE
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: com.huawei.android.launcher.permission.CHANGE_BADGE
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: com.huawei.android.launcher.permission.READ_SETTINGS
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: com.huawei.android.launcher.permission.WRITE_SETTINGS
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: android.permission.READ_APP_BADGE
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: com.oppo.launcher.permission.READ_SETTINGS
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: com.oppo.launcher.permission.WRITE_SETTINGS
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: com.cequint.ecid.CALLER_ID_LOOKUP
03-03 02:54:29.705 495 495 E DefaultPermGrantPolicy: Permission not found: com.motorola.incallui.permission.INCOMING_CALL_VISIBILITY_CHANGED
03-03 02:54:29.706 495 495 E DefaultPermGrantPolicy: Permission not found: com.google.android.setupwizard.SETUP_COMPAT_SERVICE
03-03 02:54:29.775 495 495 E DefaultPermGrantPolicy: Permission not found: com.google.android.permission.INSTALL_WEARABLE_PACKAGES
03-03 02:54:29.780 495 495 E DefaultPermGrantPolicy: Permission not found: com.google.android.googleapps.permission.GOOGLE_AUTH.mail
03-03 02:54:29.781 495 495 E DefaultPermGrantPolicy: Permission not found: com.google.android.googleapps.permission.GOOGLE_AUTH.cl
03-03 02:54:30.120 495 534 E DisplayModeDirector: Asked about unknown display, returning empty display mode specs!(id=0)
03-03 02:54:30.120 495 534 E DisplayModeDirector: Asked about unknown display, returning empty display mode specs!(id=0)
03-03 02:54:30.686 495 495 E ThermalHalWrapper: Couldn't get temperature thresholds because of HAL error: Failed to read thermal sensors.
03-03 02:54:31.055 436 466 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:31.060 436 436 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:31.162 1204 1285 E droid.bluetoot: [0303/025431.162232:ERROR:config.cc(104)] config_new: unable to open file '/data/misc/bluedroid/bt_config.conf': No such file or directory
03-03 02:54:31.162 1204 1285 E droid.bluetoot: [0303/025431.162586:ERROR:config.cc(104)] config_new: unable to open file '/data/misc/bluedroid/bt_config.bak': No such file or directory
03-03 02:54:31.162 1204 1285 E bt_btif_config_transcode: btif_config_transcode unable to load XML file '/data/misc/bluedroid/bt_config.xml': 3
03-03 02:54:31.162 1204 1285 E bt_btif_config: init unable to transcode legacy file; creating empty config.
03-03 02:54:31.188 1204 1290 E bt_btif_storage: btif_storage_get_adapter_property: Controller not ready! Unable to return Bluetooth Address
03-03 02:54:31.188 1204 1290 E BluetoothServiceJni: adapter_properties_callback: Status 1 is incorrect
03-03 02:54:31.703 443 1327 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.704 443 1327 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.707 443 443 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.707 443 443 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.715 443 443 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.717 443 443 E ion : ioctl c0044901 failed with code -1: Inappropriate ioctl for device
03-03 02:54:31.722 443 443 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.730 443 1325 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.733 443 1326 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.764 436 466 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:31.785 436 436 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:31.793 443 474 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.793 443 474 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.803 443 474 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.813 443 474 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.813 443 474 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.826 443 443 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.829 443 1335 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.840 443 1337 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.863 436 466 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:31.885 443 473 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.885 443 473 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.896 443 1327 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.917 443 1341 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.949 436 436 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:31.985 443 473 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.985 443 473 E FMQ : grantorIdx must be less than 3
03-03 02:54:31.996 443 473 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.015 443 1345 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.173 217 223 E android.system.suspend@1.0-service: Error opening kernel wakelock stats for: wakeup5: Permission denied
03-03 02:54:32.380 1228 1228 E NavigationModeController: updateCurrentInteractionMode: mode=0
03-03 02:54:32.708 217 223 E android.system.suspend@1.0-service: Error opening kernel wakelock stats for: wakeup5: Permission denied
03-03 02:54:32.793 436 436 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:32.821 436 436 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:32.852 1228 1433 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.852 1228 1433 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.853 443 1327 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.853 443 1327 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.855 1228 1433 E ion : ioctl c0044901 failed with code -1: Inappropriate ioctl for device
03-03 02:54:32.859 1228 1438 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.861 1228 1438 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.862 443 1327 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.863 443 1327 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.870 1228 1433 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.871 443 1327 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.894 1228 1438 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.895 443 1439 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.899 1228 1437 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.899 443 1314 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.935 443 1440 E FMQ : grantorIdx must be less than 3
03-03 02:54:32.936 1228 1437 E FMQ : grantorIdx must be less than 3
03-03 02:54:33.041 436 436 E Utils : did not find channel-count and/or sample-rate
03-03 02:54:33.074 1228 1450 E FMQ : grantorIdx must be less than 3
03-03 02:54:33.074 1228 1450 E FMQ : grantorIdx must be less than 3
03-03 02:54:33.076 443 473 E FMQ : grantorIdx must be less than 3
03-03 02:54:33.076 443 473 E FMQ : grantorIdx must be less than 3
03-03 02:54:33.082 1228 1450 E FMQ : grantorIdx must be less than 3
03-03 02:54:33.083 443 474 E FMQ : grantorIdx must be less than 3
03-03 02:54:33.091 443 1451 E FMQ : grantorIdx must be less than 3
03-03 02:54:33.091 1228 1437 E FMQ : grantorIdx must be less than 3
03-03 02:54:34.667 495 533 E BluetoothManagerService: MESSAGE_TIMEOUT_BIND
03-03 02:54:35.283 495 495 E TrustManagerService: EXTRA_USER_HANDLE missing or invalid, value=0
03-03 02:54:35.534 495 1309 E WindowManager: Window Session Crash
03-03 02:54:35.534 495 1309 E WindowManager: java.lang.IllegalArgumentException: Requested window null does not exist
03-03 02:54:35.534 495 1309 E WindowManager: at com.android.server.wm.WindowManagerService.windowForClientLocked(WindowManagerService.java:5443)
03-03 02:54:35.534 495 1309 E WindowManager: at com.android.server.wm.Session.actionOnWallpaper(Session.java:356)
03-03 02:54:35.534 495 1309 E WindowManager: at com.android.server.wm.Session.setWallpaperZoomOut(Session.java:382)
03-03 02:54:35.534 495 1309 E WindowManager: at android.view.IWindowSession$Stub.onTransact(IWindowSession.java:1154)
03-03 02:54:35.534 495 1309 E WindowManager: at com.android.server.wm.Session.onTransact(Session.java:139)
03-03 02:54:35.534 495 1309 E WindowManager: at android.os.Binder.execTransactInternal(Binder.java:1159)
03-03 02:54:35.534 495 1309 E WindowManager: at android.os.Binder.execTransact(Binder.java:1123)
03-03 02:54:36.081 1507 1507 E CarrierIdProvider: read carrier list from ota pb failure: java.io.FileNotFoundException: /data/misc/carrierid/carrier_list.pb: open failed: ENOENT (No such file or directory)
03-03 02:55:24.629 331 406 E display : Fail to wait requested events,numEpollEvent:-1,error:Interrupted system call
03-03 02:55:59.771 331 406 E display : Fail to wait requested events,numEpollEvent:-1,error:Interrupted system call
03-03 02:56:08.572 312 316 E IPCThreadState: attemptIncStrongHandle(3): Not supported
03-03 02:56:08.572 312 316 E IPCThreadState: attemptIncStrongHandle(68): Not supported
03-03 02:56:08.572 312 316 E IPCThreadState: attemptIncStrongHandle(46): Not supported
03-03 02:56:08.572 312 316 E IPCThreadState: attemptIncStrongHandle(18): Not supported
03-03 02:56:08.572 312 316 E IPCThreadState: attemptIncStrongHandle(47): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(61): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(33): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(48): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(42): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(44): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(66): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(26): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(11): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(19): Not supported
03-03 02:56:08.573 312 316 E IPCThreadState: attemptIncStrongHandle(32): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(29): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(63): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(62): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(54): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(37): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(8): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(39): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(65): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(23): Not supported
03-03 02:56:08.574 312 316 E IPCThreadState: attemptIncStrongHandle(25): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(56): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(15): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(13): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(49): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(24): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(51): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(58): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(60): Not supported
03-03 02:56:08.575 312 316 E IPCThreadState: attemptIncStrongHandle(17): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(52): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(30): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(4): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(50): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(35): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(38): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(7): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(16): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(9): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(64): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(27): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(21): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(41): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(55): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(40): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(34): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(28): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(20): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(36): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(31): Not supported
03-03 02:56:08.576 312 1711 E IPCThreadState: attemptIncStrongHandle(10): Not supported
03-03 02:56:08.576 312 318 E IPCThreadState: attemptIncStrongHandle(43): Not supported
03-03 02:56:08.577 312 1711 E IPCThreadState: attemptIncStrongHandle(57): Not supported
03-03 02:56:08.577 312 318 E IPCThreadState: attemptIncStrongHandle(14): Not supported
03-03 02:56:08.577 312 1711 E IPCThreadState: attemptIncStrongHandle(6): Not supported
03-03 02:56:08.577 312 318 E IPCThreadState: attemptIncStrongHandle(12): Not supported
03-03 02:56:08.577 312 1711 E IPCThreadState: attemptIncStrongHandle(5): Not supported
03-03 02:56:08.577 312 1711 E IPCThreadState: attemptIncStrongHandle(73): Not supported
03-03 02:56:08.577 312 1711 E IPCThreadState: attemptIncStrongHandle(59): Not supported
03-03 02:56:08.577 312 1760 E IPCThreadState: attemptIncStrongHandle(71): Not supported
03-03 02:56:08.577 312 1760 E IPCThreadState: attemptIncStrongHandle(1): Not supported
03-03 02:56:08.577 312 1760 E IPCThreadState: attemptIncStrongHandle(22): Not supported
03-03 02:56:08.577 312 1711 E IPCThreadState: attemptIncStrongHandle(67): Not supported
03-03 02:56:08.577 312 1760 E IPCThreadState: attemptIncStrongHandle(53): Not supported
03-03 02:56:08.577 312 1711 E IPCThreadState: attemptIncStrongHandle(69): Not supported
03-03 02:56:08.577 312 318 E IPCThreadState: attemptIncStrongHandle(2): Not supported
03-03 02:56:08.578 312 316 E IPCThreadState: attemptIncStrongHandle(45): Not supported
03-03 02:56:08.578 312 316 E IPCThreadState: attemptIncStrongHandle(70): Not supported
03-03 02:56:08.579 312 1395 E IPCThreadState: attemptIncStrongHandle(72): Not supported
03-03 02:56:09.131 1772 1772 E AudioFlinger: Failed to add event callback
03-03 02:56:09.198 1772 1815 E FastThread: did not receive expected priority boost on time
03-03 02:56:09.205 1772 1772 E APM_AudioPolicyManager: onNewAudioModulesAvailableInt: Input device list is empty!
03-03 02:56:09.207 1772 1772 E APM_AudioPolicyManager: onNewAudioModulesAvailableInt: Input device list is empty!
03-03 02:56:12.214 217 222 E android.system.suspend@1.0-service: Error opening kernel wakelock stats for: wakeup5: Permission denied
03-03 02:56:12.393 198 198 E servicemanager: Could not find android.hardware.light.ILights/default in the VINTF manifest.
03-03 02:56:14.151 437 437 E ServiceUtilities: getInfo: Cannot find package_native
03-03 02:56:43.645 331 406 E display : Fail to wait requested events,numEpollEvent:-1,error:Interrupted system call
03-03 02:57:18.033 331 406 E display : Fail to wait requested events,numEpollEvent:-1,error:Interrupted system call
03-03 02:57:26.249 1770 1770 E Zygote : Exit zygote because system server (pid 1831) has terminated
03-03 02:57:26.617 2074 2074 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.3::ISoundTriggerHw/default.
03-03 02:57:26.618 2074 2074 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.2::ISoundTriggerHw/default.
03-03 02:57:26.619 2074 2074 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.1::ISoundTriggerHw/default.
03-03 02:57:26.619 2074 2074 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.0::ISoundTriggerHw/default.
03-03 02:57:26.620 2074 2074 E LegacySupport: Could not get passthrough implementation for android.hardware.bluetooth.audio@2.0::IBluetoothAudioProvidersFactory/default.
03-03 02:57:26.621 2074 2074 E LegacySupport: Could not get passthrough implementation for android.hardware.bluetooth.a2dp@1.0::IBluetoothAudioOffload/default.
03-03 02:57:26.675 2072 2072 E Netd : Error adding route 0.0.0.0/0 -> (null) dummy0 to table 1002: File exists
03-03 02:57:26.768 2068 2068 E APM::Serializer: deserialize: Could not parse /odm/etc/audio_policy_configuration.xml document.
03-03 02:57:26.784 2068 2068 E APM::AudioPolicyEngine/Config: parse: Could not parse document /vendor/etc/audio_policy_engine_configuration.xml
03-03 02:57:26.784 2068 2068 E libxml2 : I/O warning : failed to load external entity "/vendor/etc/audio_policy_engine_configuration.xml"
03-03 02:57:26.784 2068 2068 E APM::AudioPolicyEngine/Config: parseLegacyVolumeFile: Could not parse document /odm/etc/audio_policy_configuration.xml
03-03 02:57:26.784 2068 2068 E libxml2 : I/O warning : failed to load external entity "/odm/etc/audio_policy_configuration.xml"
03-03 02:57:26.825 2074 2077 E audio_hw_primary: No supported formats: S16_LE, S24_LE and S32_LE, use default one: S16_LE
03-03 02:57:26.843 2068 2068 E AudioFlinger: Failed to add event callback
03-03 02:57:26.903 2068 2113 E FastThread: did not receive expected priority boost on time
03-03 02:57:26.910 2068 2068 E APM_AudioPolicyManager: onNewAudioModulesAvailableInt: Input device list is empty!
03-03 02:57:26.913 2068 2068 E APM_AudioPolicyManager: onNewAudioModulesAvailableInt: Input device list is empty!
03-03 02:57:27.632 2066 2066 E ActivityRecognitionHardware: activity_recognition HAL is deprecated. class_init is effectively a no-op
03-03 02:57:29.796 217 222 E android.system.suspend@1.0-service: Error opening kernel wakelock stats for: wakeup5: Permission denied
03-03 02:57:29.986 198 198 E servicemanager: Could not find android.hardware.light.ILights/default in the VINTF manifest.
03-03 02:58:00.959 331 406 E display : Fail to wait requested events,numEpollEvent:-1,error:Interrupted system call
03-03 02:58:35.182 331 406 E display : Fail to wait requested events,numEpollEvent:-1,error:Interrupted system call
03-03 02:58:43.686 2066 2066 E Zygote : Zygote failed to write to system_server FD: Connection refused
03-03 02:58:43.686 2066 2066 E Zygote : Exit zygote because system server (pid 2129) has terminated
03-03 02:58:44.058 2359 2359 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.3::ISoundTriggerHw/default.
03-03 02:58:44.059 2359 2359 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.2::ISoundTriggerHw/default.
03-03 02:58:44.060 2359 2359 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.1::ISoundTriggerHw/default.
03-03 02:58:44.061 2359 2359 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.0::ISoundTriggerHw/default.
03-03 02:58:44.061 2359 2359 E LegacySupport: Could not get passthrough implementation for android.hardware.bluetooth.audio@2.0::IBluetoothAudioProvidersFactory/default.
03-03 02:58:44.062 2359 2359 E LegacySupport: Could not get passthrough implementation for android.hardware.bluetooth.a2dp@1.0::IBluetoothAudioOffload/default.
03-03 02:58:44.116 2356 2356 E Netd : Error adding route 0.0.0.0/0 -> (null) dummy0 to table 1002: File exists
03-03 02:58:44.173 2352 2352 E APM::Serializer: deserialize: Could not parse /odm/etc/audio_policy_configuration.xml document.
03-03 02:58:44.185 2352 2352 E APM::AudioPolicyEngine/Config: parse: Could not parse document /vendor/etc/audio_policy_engine_configuration.xml
03-03 02:58:44.185 2352 2352 E libxml2 : I/O warning : failed to load external entity "/vendor/etc/audio_policy_engine_configuration.xml"
03-03 02:58:44.185 2352 2352 E APM::AudioPolicyEngine/Config: parseLegacyVolumeFile: Could not parse document /odm/etc/audio_policy_configuration.xml
03-03 02:58:44.185 2352 2352 E libxml2 : I/O warning : failed to load external entity "/odm/etc/audio_policy_configuration.xml"
03-03 02:58:44.211 0 0 E [ T161] selinux: SELinux: Could not get canonical path for /sys/devices/virtual/net/ipsec_test/queues/tx-0 restorecon: No such file or directory.
03-03 02:58:44.215 2359 2359 E audio_hw_primary: No supported formats: S16_LE, S24_LE and S32_LE, use default one: S16_LE
03-03 02:58:44.232 0 0 E [ T161] selinux:
03-03 02:58:44.235 0 0 E [ T161] ueventd: selinux_android_restorecon(/sys/devices/virtual/net/ipsec_test/queues/tx-0) failed: No such file or directory
03-03 02:58:44.252 2352 2352 E AudioFlinger: Failed to add event callback
03-03 02:58:44.318 2352 2352 E APM_AudioPolicyManager: onNewAudioModulesAvailableInt: Input device list is empty!
03-03 02:58:44.320 2352 2392 E FastThread: did not receive expected priority boost on time
03-03 02:58:44.322 2352 2352 E APM_AudioPolicyManager: onNewAudioModulesAvailableInt: Input device list is empty!
03-03 02:58:45.092 2350 2350 E ActivityRecognitionHardware: activity_recognition HAL is deprecated. class_init is effectively a no-op
03-03 02:58:47.286 217 222 E android.system.suspend@1.0-service: Error opening kernel wakelock stats for: wakeup5: Permission denied
03-03 02:58:47.459 198 198 E servicemanager: Could not find android.hardware.light.ILights/default in the VINTF manifest.
03-03 02:59:18.508 331 406 E display : Fail to wait requested events,numEpollEvent:-1,error:Interrupted system call
03-03 02:59:53.055 331 406 E display : Fail to wait requested events,numEpollEvent:-1,error:Interrupted system call
03-03 03:00:01.378 2350 2350 E Zygote : Zygote failed to write to system_server FD: Connection refused
03-03 03:00:01.379 2350 2350 E Zygote : Exit zygote because system server (pid 2412) has terminated
03-03 03:00:01.758 2641 2641 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.3::ISoundTriggerHw/default.
03-03 03:00:01.763 2641 2641 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.2::ISoundTriggerHw/default.
03-03 03:00:01.764 2641 2641 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.1::ISoundTriggerHw/default.
03-03 03:00:01.765 2641 2641 E LegacySupport: Could not get passthrough implementation for android.hardware.soundtrigger@2.0::ISoundTriggerHw/default.
03-03 03:00:01.766 2641 2641 E LegacySupport: Could not get passthrough implementation for android.hardware.bluetooth.audio@2.0::IBluetoothAudioProvidersFactory/default.
03-03 03:00:01.766 2641 2641 E LegacySupport: Could not get passthrough implementation for android.hardware.bluetooth.a2dp@1.0::IBluetoothAudioOffload/default.
03-03 03:00:01.809 2639 2639 E Netd : Error adding route 0.0.0.0/0 -> (null) dummy0 to table 1002: File exists
03-03 03:00:01.908 2636 2636 E APM::Serializer: deserialize: Could not parse /odm/etc/audio_policy_configuration.xml document.
03-03 03:00:01.920 2636 2636 E APM::AudioPolicyEngine/Config: parse: Could not parse document /vendor/etc/audio_policy_engine_configuration.xml
03-03 03:00:01.920 2636 2636 E libxml2 : I/O warning : failed to load external entity "/vendor/etc/audio_policy_engine_configuration.xml"
03-03 03:00:01.920 2636 2636 E APM::AudioPolicyEngine/Config: parseLegacyVolumeFile: Could not parse document /odm/etc/audio_policy_configuration.xml
03-03 03:00:01.920 2636 2636 E libxml2 : I/O warning : failed to load external entity "/odm/etc/audio_policy_configuration.xml"
03-03 03:00:01.943 2641 2641 E audio_hw_primary: No supported formats: S16_LE, S24_LE and S32_LE, use default one: S16_LE
03-03 03:00:01.955 2636 2636 E AudioFlinger: Failed to add event callback
03-03 03:00:02.031 2636 2674 E FastThread: did not receive expected priority boost on time
03-03 03:00:02.040 2636 2636 E APM_AudioPolicyManager: onNewAudioModulesAvailableInt: Input device list is empty!
03-03 03:00:02.043 2636 2636 E APM_AudioPolicyManager: onNewAudioModulesAvailableInt: Input device list is empty!
03-03 03:00:02.731 2634 2634 E ActivityRecognitionHardware: activity_recognition HAL is deprecated. class_init is effectively a no-op
03-03 03:00:04.809 2693 2693 E UsbAlsaJackDetectorJNI: Can't register UsbAlsaJackDetector native methods
03-03 03:00:04.922 2693 2726 E BatteryStatsService: Unable to load Power.Stats.HAL. Setting rail availability to false
03-03 03:00:04.922 2693 2726 E BluetoothAdapter: Bluetooth binder is null
03-03 03:00:04.943 217 222 E android.system.suspend@1.0-service: Error opening kernel wakelock stats for: wakeup5: Permission denied
03-03 03:00:04.945 2693 2726 E BatteryStatsService: Unable to load Power Hal or power.stats HAL
03-03 03:00:05.126 198 198 E servicemanager: Could not find android.hardware.light.ILights/default in the VINTF manifest.

 

0 件の賞賛
返信
10,837件の閲覧回数
pyh0603
Contributor III

Thank you for your reply.

Logcat is temporarily unavailable because it has not yet entered the Android system,

I have the following questions.

1. I noticed that the zygote process has been restarting, but I don't know what caused it to restart.

2. I noticed that there are several consecutive errors in the log, "init: untracked PID XXX exited with status 0". How should I debug it?

 

Looking forward to your new reply.

0 件の賞賛
返信