imx8mq configure the internal PLL as REF clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mq configure the internal PLL as REF clock

1,413 次查看
valentinraevsky
Contributor I

Dear NXP support,

We'd appreciate it if you could help in enabling the internal PLL as REF clock for the PCIe on imx8mq.

Latest good kernel 4.14.98

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/pci/dwc/pci-imx6.c?h=imx_4.14.98_2...

We'd like to have the same option on 5.4.24:

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/pci/controller/dwc/pci-imx6.c?h=re...

Let's know whether NXP is planning to bring this feature back on 5.X kernels.

We tried to make the 4.14.98 approach work on 5.4.24, but w/out any success.

Thanks in advances,

Valentin.

标签 (1)
0 项奖励
回复
2 回复数

1,377 次查看
valentinraevsky
Contributor I

Thanks it works.

0 项奖励
回复

1,405 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Valentin

 

one can try solution with "ext_osc" in dts as in boundary devices board:

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_5.4.x_2.3.0/arch/arm64/boot/dts/free...

 

Best regards
igor