imx8mq Android14 no use gki kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq Android14 no use gki kernel

1,340 Views
aber
Contributor III

Hi nxp

    Can I skip using the GKI kernel on imx8mq Android14. LOADABLE_KERNEL_MODULE = false Do not load using module mode. I have tried but the system cannot start properly.

0 Kudos
Reply
5 Replies

1,313 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

No you can't some modules are need it , such as the GPU module.

regards

0 Kudos
Reply

1,265 Views
aber
Contributor III
Hi Bio_TICFSL
There are two questions to consult:
1. The boot compiled using the no gki method has been burning in the Starting kernel .... restart
2. Does imx8MQ support mipi screen display under uboot? I checked the source code and found that imx8mm and imx8mp support it, but imx8MQ does not
0 Kudos
Reply

1,310 Views
aber
Contributor III
Hi Bio_TICFSL
Thank you for your reply. I would like to know how to run on imx8MQ without using the GKI method. Is there any specific documentation available?
0 Kudos
Reply

1,308 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

Boot.img is default GKI image, almost all build in kernel are inside this image. GKI
source code are not included in Anroid14 build environment.

Regards

0 Kudos
Reply

1,306 Views
aber
Contributor III
Yes, so I want to know if it can be achieved without GKI.
0 Kudos
Reply