imx8mq Android14 no use gki kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mq Android14 no use gki kernel

1,323 次查看
aber
Contributor III

Hi nxp

    Can I skip using the GKI kernel on imx8mq Android14. LOADABLE_KERNEL_MODULE = false Do not load using module mode. I have tried but the system cannot start properly.

0 项奖励
回复
5 回复数

1,296 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

No you can't some modules are need it , such as the GPU module.

regards

0 项奖励
回复

1,248 次查看
aber
Contributor III
Hi Bio_TICFSL
There are two questions to consult:
1. The boot compiled using the no gki method has been burning in the Starting kernel .... restart
2. Does imx8MQ support mipi screen display under uboot? I checked the source code and found that imx8mm and imx8mp support it, but imx8MQ does not
0 项奖励
回复

1,293 次查看
aber
Contributor III
Hi Bio_TICFSL
Thank you for your reply. I would like to know how to run on imx8MQ without using the GKI method. Is there any specific documentation available?
0 项奖励
回复

1,291 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

Boot.img is default GKI image, almost all build in kernel are inside this image. GKI
source code are not included in Anroid14 build environment.

Regards

0 项奖励
回复

1,289 次查看
aber
Contributor III
Yes, so I want to know if it can be achieved without GKI.
0 项奖励
回复