imx8mplus - webgl not running issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mplus - webgl not running issue

1,279 Views
bluey2ks
Contributor I

Hi,

After installing the android14.1.2 demo bsp on the imx8mplus-evk board, run webview from the main menu and enter the address threejs.org - examples menu, the first sample is not executed.

It seems that web-gl is not running normally, and when I create a webview program in android studio and upload it, the window closes with an error.

Is there anything else I need to do in the bsp settings or bsp source code to use web-gl or web-gpu?

Doesn't the GC7000UL support webgl?

 

0 Kudos
Reply
1 Reply

1,241 Views
pengyong_zhang
NXP Employee
NXP Employee
0 Kudos
Reply