imx8mplus - webgl not running issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mplus - webgl not running issue

1,240件の閲覧回数
bluey2ks
Contributor I

Hi,

After installing the android14.1.2 demo bsp on the imx8mplus-evk board, run webview from the main menu and enter the address threejs.org - examples menu, the first sample is not executed.

It seems that web-gl is not running normally, and when I create a webview program in android studio and upload it, the window closes with an error.

Is there anything else I need to do in the bsp settings or bsp source code to use web-gl or web-gpu?

Doesn't the GC7000UL support webgl?

 

0 件の賞賛
返信
1 返信

1,202件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi, @bluey2ks 

I thinks the following link can help you:

https://community.nxp.com/t5/iMX-and-Vybrid-Support/i-MX-8X-WebGL-not-working-when-using-WPE-Webkit-...

pengyong_zhang_0-1716793637525.pngpengyong_zhang_0-1716793637525.png

 

B.R

0 件の賞賛
返信