imx8mp scarthgap fetch error nnshark

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp scarthgap fetch error nnshark

1,359 Views
deepakraj
Contributor III

Hi ,

we are building scarthgap for imx8mp , we used below repo command from meta-imx .

repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.23-2.0.0.xml

 DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk source imx-setup-release.sh -b build-xwayland


when we try building image , we are facing nnshark fetch error , attached log file for reference

Resolving deltas: 100% (1839/1839), done.
Cloning into bare repository '/media/adlinkccoe29/SSD1/imx8mp/evk_imx8mp/downloads//git2/anongit.freedesktop.org.gstreamer.common'...
fatal: read error: Connection reset by peer
--2024-08-19 09:33:36-- http://downloads.yoctoproject.org/mirror/sources/git2_anongit.freedesktop.org.gstreamer.common.tar.g...
Resolving downloads.yoctoproject.org (downloads.yoctoproject.org)... 198.145.29.62
Connecting to downloads.yoctoproject.org (downloads.yoctoproject.org)|198.145.29.62|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:37 ERROR 404: Not Found.

--2024-08-19 09:33:37-- http://sources.openembedded.org/git2_anongit.freedesktop.org.gstreamer.common.tar.gz
Resolving sources.openembedded.org (sources.openembedded.org)... 198.145.29.27
Connecting to sources.openembedded.org (sources.openembedded.org)|198.145.29.27|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:38 ERROR 404: Not Found.

--2024-08-19 09:33:38-- https://mirrors.kernel.org/yocto-sources/git2_anongit.freedesktop.org.gstreamer.common.tar.gz
Resolving mirrors.kernel.org (mirrors.kernel.org)... 139.178.88.99, 2604:1380:45e3:2400::1
Connecting to mirrors.kernel.org (mirrors.kernel.org)|139.178.88.99|:443... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:39 ERROR 404: Not Found.

--2024-08-19 09:33:39-- http://downloads.yoctoproject.org/mirror/sources/git2_github.com.nxp-imx.nnshark.git.tar.gz
Resolving downloads.yoctoproject.org (downloads.yoctoproject.org)... 198.145.29.62
Connecting to downloads.yoctoproject.org (downloads.yoctoproject.org)|198.145.29.62|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:39 ERROR 404: Not Found.

--2024-08-19 09:33:39-- http://sources.openembedded.org/git2_github.com.nxp-imx.nnshark.git.tar.gz
Resolving sources.openembedded.org (sources.openembedded.org)... 198.145.29.27
Connecting to sources.openembedded.org (sources.openembedded.org)|198.145.29.27|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:40 ERROR 404: Not Found.

--2024-08-19 09:33:40-- https://mirrors.kernel.org/yocto-sources/git2_github.com.nxp-imx.nnshark.git.tar.gz
Resolving mirrors.kernel.org (mirrors.kernel.org)... 139.178.88.99, 2604:1380:45e3:2400::1
Connecting to mirrors.kernel.org (mirrors.kernel.org)|139.178.88.99|:443... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:41 ERROR 404: Not Found.


DEBUG: Python function base_do_fetch finished

DEBUG: Python function do_fetch finished

0 Kudos
Reply
1 Reply

1,319 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

nnshark should be downloaded into <build-directory>/downloads/git2/github.com.nxp-imx.nnshark.git/ from SRC_URI: GitHub - nxp-imx/nnshark: Live Profiler for NNStreamer

Don't see the full log, you can check over there, and might need to check your network, it seems with some issue about DEPENDS for downloading, like gstreamer.

Or you can try manually download it and make a copy of it.

 

Regards

Harvet

0 Kudos
Reply