imx8mp ethernet mdio clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp ethernet mdio clock

Jump to solution
748 Views
AngelF
Contributor III

Hello,

We have our own design based on imx8mp and kernel 6.6.23 from NXP.
We also have the ethernet interface, and this is the device tree configuration:

&fec {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec>;
phy-mode = "rmii";
phy-handle = <&ethphy0>;
phy-supply = <&reg_on_veth>;
status = "okay";

mdio {
#address-cells = <1>;
#size-cells = <0>;

ethphy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
nxp,rmii-refclk-in;
smsc,disable-energy-detect;
};
};
};

pinctrl_fec: fecgrp {
fsl,pins = <
MX8MP_IOMUXC_SAI1_MCLK__ENET1_TX_CLK 0x0000001f
MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x00000106
MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO 0x00000106
MX8MP_IOMUXC_SAI1_RXD4__ENET1_RGMII_RD0 0x00000091
MX8MP_IOMUXC_SAI1_RXD5__ENET1_RGMII_RD1 0x00000091
MX8MP_IOMUXC_SAI1_TXD0__ENET1_RGMII_TD0 0x0000001f
MX8MP_IOMUXC_SAI1_TXD1__ENET1_RGMII_TD1 0x0000001f
MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x0000001f
MX8MP_IOMUXC_SAI1_TXD6__ENET1_RX_ER 0x00000106
MX8MP_IOMUXC_SAI1_TXD7__ENET1_TX_ER 0x00000106
MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x00000091
>;
};

We have a problem with the "ifconfig eth0 down" command. Most of the time the signal ENET1_MDC (AH9) stays high and sometimes low.

We need to make sure that this signal goes low. When this signal is high and supply to PHY is removed, some milliamps are driven through this pin.

Best regards

Angel

0 Kudos
Reply
1 Solution
730 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

You can try to add another pinctrl handle for sleep and when the interface is down, write to the MDC pin as GPIO through filesystem.

Regards

View solution in original post

0 Kudos
Reply
2 Replies
724 Views
AngelF
Contributor III

Hello,

Thank you for your answer.

I have added pinctrl handle for sleep and it seems to drive pin to low, both when I set the interface down and when I enter standby mode.

Best regards and thank you

 

0 Kudos
Reply
731 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

You can try to add another pinctrl handle for sleep and when the interface is down, write to the MDC pin as GPIO through filesystem.

Regards

0 Kudos
Reply