imx8mp-debix-model-a.dts syntax error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp-debix-model-a.dts syntax error

2,027件の閲覧回数
qbic
Contributor I

hello,

I want to build a yocto image for the debix model a board. but when I try to compile linux-imx I get a syntax error for the corresponding .dts file

console output:

|   DTC     arch/arm64/boot/dts/freescale/imx8mp-debix-model-a.dtb
| Error: /home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/arch/arm64/boot/dts/freescale/imx8mp-debix-model-a.dts:443.4-5 syntax error
| FATAL ERROR: Unable to parse input tree
| make[3]: *** [/home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/scripts/Makefile.lib:419: arch/arm64/boot/dts/freescale/imx8mp-debix-model-a.dtb] Error 1
| make[2]: *** [/home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/scripts/Makefile.build:480: arch/arm64/boot/dts/freescale] Error 2
| make[1]: *** [/home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/Makefile:1384: freescale/imx8mp-debix-model-a.dtb] Error 2
| make: *** [/home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/Makefile:234: __sub-make] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/querner/debix-sxos/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_compile) failed with exit code '1'

 

this is the .dts file I want to use: https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mp-debix-model-...

It says syntax error on line 443.

I am quite new in the yocto eco system, so any help would be appreciated.

Best Regards.

 

0 件の賞賛
返信
2 返答(返信)

2,015件の閲覧回数
qbic
Contributor I

it seems MX8MP_IOMUXC_GPIO1_IO14__USB2_OTG_PWR is not defined.

I could only find #define MX8MP_IOMUXC_GPIO1_IO14__USB2_PWR 0x04C 0x2AC 0x000 0x1 0x0

in https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h

0 件の賞賛
返信

1,988件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @qbic!

Thank you for contacting NXP Support!

 

The problem could be that you are using our BSP for that board and our BSP is only based for our boards.

 

I recommend to check the DEBIX documentation because they should proportionate to their BSP for their board.

 

https://debix.io/Document/manual/id/1.html

 

Sorry for the mistake!


Best Regards!

Chavira

0 件の賞賛
返信