imx8mp crash during bootup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mp crash during bootup

1,104 次查看
jiangyaqiang
Senior Contributor I

HI anyone:

 

My imx8mp board sometimes fail to bootup, it crash/stop in the kernel. When it stops, it's no error log.

the enviroment is :

kernel :5.4.70

system: yocto-5.4.70

ddr stress test is ok for over night test.

I attach some log bellow, the detail log is in the attachment.

[ 4.772269] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 4.780889] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 25.787874] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 25.793972] rcu: 2-...0: (1 GPs behind) idle=8e6/1/0x4000000000000000 softirq=152/153 fqs=2360
[ 25.802756] (detected by 0, t=5255 jiffies, g=-879, q=17)
[ 25.808240] Task dump for CPU 2:
[ 25.811467] swapper/0 R running task 0 1 0 0x0000002a
[ 25.818516] Call trace:
[ 25.820968] __switch_to+0x108/0x1c0
[ 25.824543] 0xffff80001003bca8

 

Any help will be appreciative.

Best regards.

标签 (1)
0 项奖励
回复
0 回复数