imx8mp boot nfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp boot nfs

1,376 Views
itamarlevit
Senior Contributor I

Hi support 

When I boot with SDK it OK 

but when I try to boot with NFS it fail or take allot of time 

setenv kernel Image
setenv fdt_file imx8mp-evk.dtb
setenv fdt_addr 0x40480000
setenv kernel_addr 0x43000000
setenv bootargs_base 'setenv bootargs console=ttymxc1,115200 root=/dev/nfs ip=192.168.0.45 192.168.0.115:/home/develop/rootfs,v3,tcp clk_ignore_unused'
setenv bootargs_base 'setenv bootargs console=ttymxc1,115200 root=/dev/mmcblk1p2 rootwait rw clk_ignore_unused'
setenv bootcmd_mmc 'run bootargs_base; fatload mmc 1 ${kernel_addr} ${kernel}; fatload mmc 1 ${fdt_addr} ${fdt_file};'
setenv bootcmd 'run bootcmd_mmc; booti ${kernel_addr} - ${fdt_addr};'
saveenv

 

 

0 Kudos
Reply
1 Reply

1,365 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi ,

 

   i.MX8MP hasn't officially been released yet, so refer to "Boot i.MX8MM using NFS", please!

https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX8MM-using-NFS/td-p/1152978

 

Hope this information is helpful for you.

Have a nice day!

B.R,

Weidong

0 Kudos
Reply