imx8mp android gstreamer hw decode and encode plugin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp android gstreamer hw decode and encode plugin

2,787 Views
kevin3_wei
Contributor I

Hi:

  We want to use gstreamer command in imx8mp android 11, so i have use cerbero to cross compile gstreamer, but after cross compile done , i cannot found vpuenc_h264 and vpudec plugin when run gst-inspect-1.0, how to add imx8mp hardware decode and encode  plugin into cerbero?

 

   https://gstreamer.freedesktop.org/documentation/installing/building-from-source-using-cerbero.html?g...

Thanks

0 Kudos
Reply
2 Replies

2,342 Views
sig0912
Contributor III

Hi @kevin3_wei 

I am running into the same issue. I am using imx8qm with Android 12 and I am trying to install gstreamer into the system.

When I run gst-launch-1.0 v4l2src... it does not find the plugin v4l2src.

Did you get the chance to fix this issue? If so how did you install the plugins into the Android system?

Thanks,

0 Kudos
Reply

2,722 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Please refer to Table 16.i.MX GStreamer 1.0 plugins in i.MX Linux Release Notes for supported video encoder and decoder plug-ins in i.MX8MP.
 
Please refer to 7.3.3 Video encoding in i.MX Linux User's Guide
 
One can use v4l2h264enc, v4l2h265enc and v4l2h264dec,v4l2h265dec for i.MX 8M Plus.
 
Thanks &  Regards,
Sanket Parekh
0 Kudos
Reply