[imx8mp][android] WebGL Aquarium rendering issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[imx8mp][android] WebGL Aquarium rendering issue

跳至解决方案
801 次查看
jason9816
Contributor I

As the title says, we encountered flickering and graphical issues when running the WebGL Aquarium demo on our NXP i.MX8MP SoC custom board with Android 12-15. I also tested it on an NXP i.MX8MP EVK board with the 15.0.0_1.0.0_DEMO_8MP Android prebuilt images, and the issue remains.

Previously, we tested the same setup on our NXP i.MX8MP SoC custom board running Android 12-14 about a year ago, and it was working fine at that time. However, the issue seems to have appeared this year.

We have attached a recording from our NXP i.MX8MP SoC custom board running Android 15 to showing the issue.

IMX8MPLUS 

0 项奖励
回复
1 解答
735 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Correct! is a known issue on Android devices.

Regards

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
774 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Weston is one process using GPU. It's able to see chromium-bin in the process list of gputop also. When browsering "webglsamples.org/aquarium/aquarium.html", we can see GPU usage going high.

If chromium runs with "chromium --no-sandbox --disable-gpu", we can observe chromium-bin is not in GPU process list and usage is null. Also the web shows empty with "webglsamples.org/aquarium/aquarium.html". That proves GPU is enabled without "--disable-gpu".

 

regards

0 项奖励
回复
759 次查看
jason9816
Contributor I

Hello,

Yes, I have tested it on our Yocto 5.0 OS, and it worked fine. The flickering issue seems to occur only on Android. Is this a known issue on Android?

 

regards

0 项奖励
回复
736 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Correct! is a known issue on Android devices.

Regards

 

0 项奖励
回复