imx8mp CSI-2 frame start issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8mp CSI-2 frame start issue

跳至解决方案
7,748 次查看
Jayden_Soon
Contributor I

I am developing a 2-channel camera with DART-MX8M-PLUS.

CAM -> PR2000K(HD Receiver with MIPI output) -> imx8mp

PR2000K only supports clock continuous mode. No non-continuous mode.

csi2-0 works normally, but csi2-1 cannot get a start frame. Strangely, sometimes it works.

Below are the dts file settings.

pr2000k_mipi1: pr2000k_mipi@5c {
  compatible = "pixelplus,pr2000k";
  reg = <0x5c>;
  clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
  clock-names = "xclk";
  csi_id = <1>;
  mipi_csi;
  status = "okay";

  port {
    pr2000k_mipi_1_ep: endpoint {
    remote-endpoint = <&mipi_csi1_ep>;
    data-lanes = <1 2 3 4>;
    clock-lanes = <0>;
  };
 };
};

pr2000k_mipi0: pr2000k_mipi@5f {
  compatible = "pixelplus,pr2000k";
  reg = <0x5f>;
  clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
  clock-names = "xclk";
  csi_id = <0>;
  mipi_csi;
  status = "okay";

  port {
    pr2000k_mipi_0_ep: endpoint {
    remote-endpoint = <&mipi_csi0_ep>;
    data-lanes = <1 2 3 4>;
    clock-lanes = <0>;
  };
 };
};

&mipi_csi_0 {
  #address-cells = <1>;
  #size-cells = <0>
  status = "okay";

  port@0 {
    reg = <0>;
    mipi_csi0_ep: endpoint {
    remote-endpoint = <&pr2000k_mipi_0_ep>;
    data-lanes = <4>;
    csis-hs-settle = <3>;
    csis-clk-settle = <0>;
    csis-wclk;
  };
 };
};

&mipi_csi_1 {
  #address-cells = <1>;
  #size-cells = <0>
  status = "okay";

  port@1 {
    reg = <1>;
    mipi_csi1_ep: endpoint {
    remote-endpoint = <&pr2000k_mipi_1_ep>;
    data-lanes = <4>;
    csis-hs-settle = <3>;
    csis-clk-settle = <0>;
    csis-wclk;
  };
 };
};

 

Debug message of imx8-mipi-csi2-sam.c

csi2-1 cannot get a start frame like below.

[ 167.160218] mxc-mipi-csi2.0: mipi_csis_s_stream: 1, state: 0x0
[ 167.160329] mxc-mipi-csi2.0: mipi_csis_imx8mp_phy_reset: bus fmt is 12 bit !
[ 167.160368] mxc-mipi-csi2.0: fmt: 0x2006, 1280 x 960
[ 167.160405] mxc-mipi-csi2.0: Frame Start: 1
[ 167.160410] mxc-mipi-csi2.0: status: 01000000
[ 167.176222] mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
[ 167.176234] mxc-mipi-csi2.0: CSIS_VERSION[0]: 0x03060301
[ 167.176241] mxc-mipi-csi2.0: CSIS_CMN_CTRL[4]: 0x00004b05
[ 167.176247] mxc-mipi-csi2.0: CSIS_CLK_CTRL[8]: 0x000f0000
[ 167.176252] mxc-mipi-csi2.0: CSIS_INTMSK[10]: 0x0fffff1f
[ 167.176258] mxc-mipi-csi2.0: CSIS_INTSRC[14]: 0x00000000
[ 167.176264] mxc-mipi-csi2.0: CSIS_DPHYSTATUS[20]: 0x00000000
[ 167.176270] mxc-mipi-csi2.0: CSIS_DPHYCTRL[24]: 0x0300001f
[ 167.176276] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_L[30]: 0x000001f4
[ 167.176283] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_H[34]: 0x00000000
[ 167.176289] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_L[38]: 0x00000000
[ 167.176295] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_H[3c]: 0x00000000
[ 167.176301] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH0[40]: 0x00001078
[ 167.176306] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH1[50]: 0x000008fd
[ 167.176313] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH2[60]: 0x000008fe
[ 167.176319] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH3[70]: 0x000008ff
[ 167.176325] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH0[44]: 0x03c00500
[ 167.176330] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH1[54]: 0x80008000
[ 167.176336] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH2[64]: 0x80008000
[ 167.176342] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH3[74]: 0x80008000
[ 167.176348] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH0[48]: 0x00000000
[ 167.176354] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH1[58]: 0x00000000
[ 167.176359] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH2[68]: 0x00000000
[ 167.176365] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH3[78]: 0x00000000
[ 167.176371] mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
[ 167.176376] mxc-mipi-csi2.0: GPR_GASKET_0_CTRL[60]: 0xffff8000
[ 167.176384] mxc-mipi-csi2.0: GPR_GASKET_0_HSIZE[64]: 0xffff8000
[ 167.176389] mxc-mipi-csi2.0: GPR_GASKET_0_VSIZE[68]: 0xffff8000
[ 167.192412] mxc-mipi-csi2.0: Frame End: 1
[ 167.192426] mxc-mipi-csi2.0: status: 00100000
[ 167.193739] mxc-mipi-csi2.0: Frame Start: 2
[ 167.193752] mxc-mipi-csi2.0: status: 01000000
[ 167.225753] mxc-mipi-csi2.0: Frame End: 2
[ 167.225768] mxc-mipi-csi2.0: status: 00100000
[ 167.227075] mxc-mipi-csi2.0: Frame Start: 3
[ 167.227090] mxc-mipi-csi2.0: status: 01000000
[ 202.392216] mxc-mipi-csi2.1: mipi_csis_s_stream: 1, state: 0x0
[ 202.392333] mxc-mipi-csi2.1: mipi_csis_imx8mp_phy_reset: bus fmt is 12 bit !
[ 202.392372] mxc-mipi-csi2.1: fmt: 0x2006, 1280 x 960
[ 202.408216] mxc-mipi-csi2.1: --- mipi_csis_s_stream ---
[ 202.408228] mxc-mipi-csi2.1: CSIS_VERSION[0]: 0x03060301
[ 202.408235] mxc-mipi-csi2.1: CSIS_CMN_CTRL[4]: 0x00004b05
[ 202.408241] mxc-mipi-csi2.1: CSIS_CLK_CTRL[8]: 0x000f0000
[ 202.408246] mxc-mipi-csi2.1: CSIS_INTMSK[10]: 0x0fffff1f
[ 202.408252] mxc-mipi-csi2.1: CSIS_INTSRC[14]: 0x00000000
[ 202.408258] mxc-mipi-csi2.1: CSIS_DPHYSTATUS[20]: 0x000000f2
[ 202.408266] mxc-mipi-csi2.1: CSIS_DPHYCTRL[24]: 0x0300001f
[ 202.408271] mxc-mipi-csi2.1: CSIS_DPHYBCTRL_L[30]: 0x000001f4
[ 202.408279] mxc-mipi-csi2.1: CSIS_DPHYBCTRL_H[34]: 0x00000000
[ 202.408285] mxc-mipi-csi2.1: CSIS_DPHYSCTRL_L[38]: 0x00000000
[ 202.408291] mxc-mipi-csi2.1: CSIS_DPHYSCTRL_H[3c]: 0x00000000
[ 202.408296] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH0[40]: 0x00001078
[ 202.408302] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH1[50]: 0x000008fd
[ 202.408308] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH2[60]: 0x000008fe
[ 202.408314] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH3[70]: 0x000008ff
[ 202.408322] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH0[44]: 0x03c00500
[ 202.408327] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH1[54]: 0x80008000
[ 202.408335] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH2[64]: 0x80008000
[ 202.408341] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH3[74]: 0x80008000
[ 202.408347] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH0[48]: 0x00000000
[ 202.408353] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH1[58]: 0x00000000
[ 202.408358] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH2[68]: 0x00000000
[ 202.408365] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH3[78]: 0x00000000
[ 202.408371] mxc-mipi-csi2.1: --- mipi_csis_s_stream ---
[ 202.408376] mxc-mipi-csi2.1: GPR_GASKET_0_CTRL[60]: 0xffff8000
[ 202.408382] mxc-mipi-csi2.1: GPR_GASKET_0_HSIZE[64]: 0xffff8000
[ 202.408388] mxc-mipi-csi2.1: GPR_GASKET_0_VSIZE[68]: 0xffff8000

 

https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-dual-MIPI-camera-CSI-2-1-not-leaving-ULPS-s... 

This is similar to the post above.

Are both 2 channels not captured in continuous mode?

Should I redesign with a different receiver chip?

Thanks in advance.

Best regards,

Jayden

 

0 项奖励
回复
1 解答
7,596 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Jayden_Soon,

I hope you are doing well.
 
Both continuous and non-continuous modes are supported on IMX8MP. But as mentioned in the document AN13857 section 6.4 Debug tips,
 
"Note: i.MX 8MM, i.MX 8MN, and i.MX 8MP require the connected camera to work in the LP state before
enabling the Rx DPHY. But if the camera works in continuous clock mode, the clock lane may always be in the
HS mode. In this case, Rx DPHY may not detect the HS mode and wrongly remains in the stop or ULPS state."
 
Hence, it is recommended to use the clock in non-continuous mode.
 
Thanks & Regards,
Sanket Parekh

在原帖中查看解决方案

0 项奖励
回复
6 回复数
5,097 次查看
Rosan
Contributor I
Hi @Jayden_Soon,

I hope you are doing well.
I am currently working with the PR2000K MIPI camera. If you have the Linux driver code for the PR2000K, it would be very helpful to me.

Thank you!
0 项奖励
回复
7,690 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
Kindly mention your BSP version.
Are you using the csi2-0 and csi2-1 simultaneously?
 
Thanks & Regards,
Sanket Parekh
0 项奖励
回复
7,678 次查看
Jayden_Soon
Contributor I

Hi Sanket,

SOM : DART-MX8M-PLUS

BSP : Yocto mx8mp-yocto-kirkstone-5.15-2.0.x-v1.2

I'm trying to use the csi2-0 and csi2-1 simultaneously.

Thanks.

Best regards,

Jayden

 

 

0 项奖励
回复
7,597 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Jayden_Soon,

I hope you are doing well.
 
Both continuous and non-continuous modes are supported on IMX8MP. But as mentioned in the document AN13857 section 6.4 Debug tips,
 
"Note: i.MX 8MM, i.MX 8MN, and i.MX 8MP require the connected camera to work in the LP state before
enabling the Rx DPHY. But if the camera works in continuous clock mode, the clock lane may always be in the
HS mode. In this case, Rx DPHY may not detect the HS mode and wrongly remains in the stop or ULPS state."
 
Hence, it is recommended to use the clock in non-continuous mode.
 
Thanks & Regards,
Sanket Parekh
0 项奖励
回复
7,584 次查看
Jayden_Soon
Contributor I

Hi Sanket,

PR2000K(HD Receiver) only supports clock continuous mode.

It's hard to solve it and looks like I need a little more study.

Thank you for reply.

Best regards,

Jayden

 

0 项奖励
回复
7,558 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Is there any update from your side?
If there isn't any query should I proceed to close this thread?
 
Thanks & Regards
Sanket Parekh

0 项奖励
回复