[imx8mp] 256MB of memory wasted in default dtsi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[imx8mp] 256MB of memory wasted in default dtsi

ソリューションへジャンプ
1,466件の閲覧回数
martinetd
Contributor IV

Hello,

 

The imx8mp.dtsi device tree include shipped in https://github.com/nxp-imx/linux-imx (all branches) defined a `isp0_reserved` memory region which is unmapped by linux even if isp0 itself is disabled.

Disabling the memory region immediately frees up 256MB of memory (just disabling the node is enough, see below patch)

The comment immediately above states "used only by tuning tool, can be removed for normal case" so there probably is no reason to keep it enabled by default, please report this to whomever if may concern (the linux upstream dtsi does not contain this section)

 

 

 

From c26321365174d71cf8642f309f16eeefda36c7c9 Mon Sep 17 00:00:00 2001
From: Dominique Martinet <dominique.martinet@atmark-techno.com>
Date: Fri, 28 Apr 2023 12:48:47 +0900
Subject: [PATCH] arm64: imx8mp.dtsi: disable isp0_reserved by default

isp0_reserved is 256MB big and described as "used only by tuning tool,
can be removed for normal case": so disable it by default,
and anyone enabling isp0 must enable the reserved memory as well
manually
(why wouldn't linux automatically do this...)

This increases the available memory on Armadillo IoT G4 as confirmed
below.

Before:
armadillo:~# free -m
       total        used        free      shared  buff/cache   available
Mem:    1668         884         209          67         575         629

After:
armadillo:~# free -m
       total        used        free      shared  buff/cache   available
Mem:    1924         341        1531           1          52        1524

Signed-off-by: Dominique Martinet <dominique.martinet@atmark-techno.com>
---
 arch/arm64/boot/dts/freescale/imx8mp.dtsi | 1 +
 1 file changed, 1 insertion(+)

diff --git a/arch/arm64/boot/dts/freescale/imx8mp.dtsi b/arch/arm64/boot/dts/freescale/imx8mp.dtsi
index dccf24c90862..dde207a7f348 100755
--- a/arch/arm64/boot/dts/freescale/imx8mp.dtsi
+++ b/arch/arm64/boot/dts/freescale/imx8mp.dtsi
@@ -217,6 +217,7 @@ dsp_vdev0buffer: vdev0buffer@94300000 {
 		isp0_reserved: isp0@94400000 {
 			no-map;
 			reg = <0 0x94400000 0 0x10000000>;
+			status = "disabled";
 		};
 	};
 
-- 
2.39.2

 

 

 

Thanks.

0 件の賞賛
返信
1 解決策
1,344件の閲覧回数
martinetd
Contributor IV

I see it's been removed in the latest BSP (lf-6.1.22-2.0.0, in commit https://github.com/nxp-imx/linux-imx/commit/910178d16dd3e4cba08bebde148c493308cd3fd7 )

Thanks

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,437件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
It is true that the reserved memory node will reserve memory irrespective of the status of the isp node.
 
One can disable it for normal use cases.
 
I will inform the internal team regarding this case.
 
Thanks & Regards,
Sanket Parekh
1,345件の閲覧回数
martinetd
Contributor IV

I see it's been removed in the latest BSP (lf-6.1.22-2.0.0, in commit https://github.com/nxp-imx/linux-imx/commit/910178d16dd3e4cba08bebde148c493308cd3fd7 )

Thanks

0 件の賞賛
返信