imx8mn no network messages in sleep mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mn no network messages in sleep mode

1,293 次查看
mudherp
Contributor IV

Hi

We have the tcp/ip stack up and running by default on our ui board that uses the imx8mn.
We put the board to sleep using the following command:

echo "s2idle" > /sys/power/mem_sleep
echo mem > /sys/power/state

After we have issued the command we have monitored using wireshark the the router send an ARP message to the ui board. But the ui board does not respond to the arp message.

From the above the router sends ARP message to the ui board for at over 10 minutes. Eventually the router removes the ui board from it attached devices.

Hence if we ping the ui board it is un-reachable.

So is their a way to keep the ip stack alive when the imx8mn is asleep?

0 项奖励
回复
4 回复数

1,262 次查看
opedis
Contributor III

There is no way to do that. 

Only way is using Wake-on-LAN ( WoL) . 

0 项奖励
回复

1,232 次查看
mudherp
Contributor IV

Please tell me how Wake-on-LAN ( WoL) works and how do i enable it for imx8mn-evk

 

0 项奖励
回复

1,246 次查看
mudherp
Contributor IV

Please tell me how Wake-on-LAN ( WoL) works and how do i enable it for imx8mn-evk

0 项奖励
回复

1,278 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @mudherp 

It's hard to realize this feature, need to modify much frameworks if we add this.

You can contact SE team for this.

Best Regards

Zhiming

0 项奖励
回复