imx8mmevk - Enabling the secure boot support in U-Boot - Unable to find defconfig & Kconfig files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mmevk - Enabling the secure boot support in U-Boot - Unable to find defconfig & Kconfig files

1,178件の閲覧回数
autoamp
Contributor III

Hello Team,

Am trying to implement and verify secure boot on imx8mmevk.

with reference to i.MX8M family Secure Boot guide using HABv4, we need to enable secure boot support in U-Boot by doing two tasks.

  • Defconfig: CONFIG_IMX_HAB=y
  • Kconfig: ARM architecture -> Support i.MX HAB features

Unfortunately am unable to find those files in my build-env.

Currently we are using yocto project for building images.

- I looked under dir /meta-imx/meta-bsp/conf/machine for editing machine file. It didn't worked? What am I missing here?

Ref:

i.MX8M family Secure Boot guide using HABv4 

- AN12312

タグ(1)
0 件の賞賛
返信
1 返信

1,164件の閲覧回数
Yuri
NXP Employee
NXP Employee

@autoamp 
Hello,

  It is needed to add "CONFIG_IMX_HAB=y" to Your defconfig file  (imx8mm_evk_defconfig).

Regards,
Yuri.

0 件の賞賛
返信