imx8mmevk - Enabling the secure boot support in U-Boot - Unable to find defconfig & Kconfig files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mmevk - Enabling the secure boot support in U-Boot - Unable to find defconfig & Kconfig files

1,226 Views
autoamp
Contributor III

Hello Team,

Am trying to implement and verify secure boot on imx8mmevk.

with reference to i.MX8M family Secure Boot guide using HABv4, we need to enable secure boot support in U-Boot by doing two tasks.

  • Defconfig: CONFIG_IMX_HAB=y
  • Kconfig: ARM architecture -> Support i.MX HAB features

Unfortunately am unable to find those files in my build-env.

Currently we are using yocto project for building images.

- I looked under dir /meta-imx/meta-bsp/conf/machine for editing machine file. It didn't worked? What am I missing here?

Ref:

i.MX8M family Secure Boot guide using HABv4 

- AN12312

Tags (1)
0 Kudos
Reply
1 Reply

1,212 Views
Yuri
NXP Employee
NXP Employee

@autoamp 
Hello,

  It is needed to add "CONFIG_IMX_HAB=y" to Your defconfig file  (imx8mm_evk_defconfig).

Regards,
Yuri.

0 Kudos
Reply