imx8mm yotoc qt5 build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm yotoc qt5 build error

1,410 Views
blackhuang
Contributor I

在使用imx8mm在线构建yocto时出现如下问题,不知道什么原因?谢谢!

cd qtbench/ && ( test -e Makefile || /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/git/tests/benchmarks/gui/painting/qtbench/qtbench.pro -qtconf /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/bin/qt.conf ) && make -f Makefile
| make[2]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/auto'
| Makefile:45: recipe for target 'sub-auto-make_first' failed
| make[1]: *** [sub-auto-make_first] Error 2
| make[1]: *** Waiting for unfinished jobs....
| cd text/ && ( test -e Makefile || /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/git/tests/benchmarks/gui/text/text.pro -qtconf /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/bin/qt.conf ) && make -f Makefile
| make[5]: Entering directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/painting/qtransform'
| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/painting/qtransform'
| make[4]: Entering directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/text'
| cd qfontmetrics/ && ( test -e Makefile || /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/git/tests/benchmarks/gui/text/qfontmetrics/qfontmetrics.pro -qtconf /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/bin/qt.conf ) && make -f Makefile
| cd qtext/ && ( test -e Makefile || /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/git/tests/benchmarks/gui/text/qtext/qtext.pro -qtconf /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/bin/qt.conf ) && make -f Makefile
| make[5]: Entering directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/styles/qstylesheetstyle'
| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/styles/qstylesheetstyle'
| make[4]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/styles'
| cd qtextdocument/ && ( test -e Makefile || /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/git/tests/benchmarks/gui/text/qtextdocument/qtextdocument.pro -qtconf /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/bin/qt.conf ) && make -f Makefile
| make[5]: Entering directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/painting/qtbench'
| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/painting/qtbench'
| make[4]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/painting'
| make[5]: Entering directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/text/qfontmetrics'
| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/text/qfontmetrics'
| make[5]: Entering directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/text/qtext'
| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/text/qtext'
| make[5]: Entering directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/text/qtextdocument'
| make[5]: Nothing to be done for 'first'.
| make[5]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/text/qtextdocument'
| make[4]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui/text'
| make[3]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks/gui'
| make[2]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests/benchmarks'
| make[1]: Leaving directory '/home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/build/tests'
| Makefile:98: recipe for target 'sub-tests-make_first' failed
| make: *** [sub-tests-make_first] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/fushi/imx-yocto-bsp/build-wayland/tmp/work/aarch64-mx8mm-poky-linux/qtbase/5.10.1+gitAUTOINC+6c6ace9d23-r0/temp/log.do_compile.19758)
ERROR: Task (/home/fushi/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6677 tasks of which 6671 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/fushi/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

Labels (1)
0 Kudos
Reply
0 Replies