According to the MIPI CSI2 D-PHY specification shown below, the minimum Ths_settle = 85ns + 6UI and the maximum Ths_settle = 145ns + 10UI, where UI is the period the HS data rate on the MIPI CSI data lanes, since the high speed (HS) data is transmitted in DDR (rising edge and falling edge of the clock) mode, 1 UI = 1/2 period of the MIPI CSI HS clock.


In calculation of the Ths_setttle, the HSSTTEL bit field is combined with the period of the LP clock whose maximum frequency is 10MHz, its period (Tlp) is 100ns then. That is Ths_settle = Tlp + Tlp / HSSETTL[7:0] = 100ns + 100ns / HSSETTL[7:0].
The "MIPI Serial clock Frequency (MHz)" in the Excel table shall be modified as "MIPI Serial data rate (Mbps)". That is the MIPI CSI HS clock frequency is half of the MIPI serial data rate. The minimum data rate of the MIPI CSI D-PHY is 80Mbps and the maximum data rate is 1500Mbps.
You shall set the HSSETTLE[7:0] bit field according to the actual MIPI CSI HS clock frequency setting.
If the MIPI CSI HS clock frequency is 150MHz, that means the data rate is 300Mbps and it shall be set as HSSETTLE[7:0] = 6 for Ths_settle = 100ns + 100ns / 6 = 117ns. It meets the requirement of [85ns + 6UI = 85ns + 6 x 1000ns / 300 = 105ns] < Ths_settle < [45ns + 10UI = 145ns + 10 x 1000ns / 300 = 178ns].