Hi,
I use advantech-ROM5721 and I face a problem about porting audio codec SGTL5000.
I set the codec sys_mclk to 24,576,000Hz and use codec internal PLL function descripte in datasheet Figure 9.
Here is device tree and driver I use.
The HP_Out and Line_Out output with a lot of noise (sounds likewhite noise).
I try some modify to fix the problem but unfortunately.
What I try
1. regard frequecny(24,576,000Hz) as 22579200 to setup the CHIP_CLK_CTRL register (as attachment line 965)
The noise almost cancel, but the tone different about 10%
Ex I play 1KHz single tone sound, output 1.09KHz tone.
2. change sys_clk to 22,579,200 (44,100Hz*512) at the device tree as below.
&sai1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai1>;
assigned-clocks = <&clk IMX8MM_CLK_SAI1>;
assigned-clock-parents = <&clk IMX8MM_AUDIO_PLL1_OUT>;
// assigned-clock-rates = <0>, <24576000>;
assigned-clock-rates = <0>, <22579200>;
status = "okay";
};
&i2c4{
codec: sgtl5000@a {
compatible = "fsl,sgtl5000";
reg = <0x0a>;
clocks = <&clk IMX8MM_CLK_SAI1_ROOT>;
clock-names = "mclk";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai1_mclk>;
assigned-clocks = <&clk IMX8MM_CLK_SAI1>;
assigned-clock-parents = <&clk IMX8MM_AUDIO_PLL1_OUT>;
// assigned-clock-rates = <24576000>;
assigned-clock-rates = <22579200>;
};
};
The driver only apply frequency to 23,130,353 Hz
I use printk in the function "sgtl5000_set_dai_sysclk " to check sysclk
Since the mclk/sample_freq is not equal to 256, 384 or 512, driver use the PLL setting.
What is the sysclk prefre for sgtl5000?
How to change the sysclk to specific frequency(ex:22,579,200 (44,100Hz*512) or 11,289,600(44,100Hz*256))?