imx8mm TMU not working in uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8mm TMU not working in uboot

跳至解决方案
1,295 次查看
borysszefler
Contributor II

I have imx8mm on custom SOM and I'm running nxp uboot_imx(lf_v2022.04). Internal temperature sensor is not working as expected on multiple tested devices.
It displays only this string without actual temperature value:

CPU: Industrial temperature grade (-40C to 105C)

Uboot debugging showed that probably temperature value is out of range. (sensor range is 10-125). Return code of thermal_get_temp function (cpu.c) is -22(EINVAL).

I tried to read registers and the output is:

TMU_TSCR register value: 2147483657
TRITSR register value: 0

TSCR suggests that value is beyond range.

What can cause this issue?

标签 (1)
0 项奖励
回复
1 解答
1,274 次查看
borysszefler
Contributor II

It turned out that I had wrong resistor value on TSENSOR_RES_EXT line. Solution was found on this old thread https://community.nxp.com/t5/i-MX-Processors/thermal-zone0-Resource-temporarily-unavailable/td-p/108....

I tried to confirm this but could not find this information in hardware design guidelines nor other imx8mm documentation.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,275 次查看
borysszefler
Contributor II

It turned out that I had wrong resistor value on TSENSOR_RES_EXT line. Solution was found on this old thread https://community.nxp.com/t5/i-MX-Processors/thermal-zone0-Resource-temporarily-unavailable/td-p/108....

I tried to confirm this but could not find this information in hardware design guidelines nor other imx8mm documentation.

0 项奖励
回复