imx8mm FlexSPI id error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm FlexSPI id error

Jump to solution
3,808 Views
jianfeichang
Contributor IV

imx8mm linux 4.14.98 kernel log:

[ 1.683298] loop: module loaded
[ 1.690477] fsl-flexspi 30bb0000.flexspi: unrecognized JEDEC id bytes: 00, 00, 00
[ 1.697985] fsl-flexspi 30bb0000.flexspi: Freescale FlexSPI probe failed
[ 1.704759] fsl-flexspi: probe of 30bb0000.flexspi failed with error -2
[ 1.711483] slram: not enough parameters.

it is MT25QL256ABA,8MA15 RW163 。

pastedImage_1.png

pastedImage_2.png

fsl-imx8mm-evk.dts:

&flexspi {
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_flexspi0>;
   status = "okay";

   flash0: mt25qu256aba@0 {
   reg = <0>;
   #address-cells = <1>;
   #size-cells = <1>;
   compatible = "micron,mt25qu256aba";
   spi-max-frequency = <80000000>;
   spi-nor,ddr-quad-read-dummy = <6>;
};
};

root@imx8mmevk:~# cat /proc/mtd
dev: size erasesize name
root@imx8mmevk:~#

can you help me?

Labels (1)
0 Kudos
Reply
1 Solution
3,659 Views
igorpadykov
NXP Employee
NXP Employee

Hi jianfei

MT25QL256ABA is 2.7-3.6V according to its datasheet

https://www.micron.com/-/media/client/global/documents/products/data-sheet/nor-flash/serial-nor/mt25... 

EVK uses 1.7-2.0V  MT25QU256ABA1EW7 part.

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
3,660 Views
igorpadykov
NXP Employee
NXP Employee

Hi jianfei

MT25QL256ABA is 2.7-3.6V according to its datasheet

https://www.micron.com/-/media/client/global/documents/products/data-sheet/nor-flash/serial-nor/mt25... 

EVK uses 1.7-2.0V  MT25QU256ABA1EW7 part.

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,659 Views
jianfeichang
Contributor IV

Hi igorpadykov

      You're right.!Thank you very much!it is 2.7-3.6V!

0 Kudos
Reply