imx8mini emmc efuse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mini emmc efuse

8,903件の閲覧回数
tarterkit_ru
Contributor III

Hello, i want burn efuse on imx8mini for emmc boot, emmc connected exactly like EVK board (SD3 8 bit on NAND pins), can you tell me arguments of uboot like:

fuse prog [-y] <bank> <word> <hexval> [<hexval>...]

ラベル(1)
7 返答(返信)

7,301件の閲覧回数
frix
Contributor II

Good day,

Have you managed to solve your e-Fuse boot problem?

I'm successfully using the Super Root Key to boot a signed u-boot. I'm trying to lock down the boot sequence to only use the eMMC. There's also a fallback to SD if the DISABLE_SDMMC_MFG bit is left at 0.

Before setting the fuses I've used the development kits external boot select switches to successfully boot from SD and eMMC.

The iMX 8M Mini application processor reference manual was used to look up the
meaning of the register definitions.

OCOTP_HW_OCOTP_BOOT_CFG0 register:
3035_0470 Value of OTP Bank1 Word3

Register fields defined on page 823 & p824
[15: 0] BOOT_CFG
     Page 816: Boot fusemap : eMMC
     [0] - IO voltage selection (Manufacture mode) : 0=3V3
     [1] - IO voltage selection (Normal boot mode) : 0=3V3
     [3:2] - Speed : 00=Normal
     [6:4] - Bus width : 010=8-bit
     [7] - Fast boot: 0=Regular
     [8] - SD loopback : 0=Through SD pad
     [9] - Power cycle : 0=Disable
     [11:10]- Port select : 10=uSDHC3
     [14:12]- Boot device select : 010=eMMC (According to p815, Table 6-41)
     [15] - Reserved
[24:16] Reserverd
[25] SEC_CONFIG[1] : 1x - Closed (HAB Security On)
[27:26] Reserved
[28] BT_FUSE_SEL : 1=Boot config from eFuses
[29] FORCE_COLD_BOOT : 1=Always cold boot. Higher security
[31:30] Reserved

The programmed fuse value:
u-boot=> fuse sense 1 3 1
    Sensing bank 1:
    Word 0x00000003: 0x32002820

When u-boot is programmed into eMMC, it boots it regardless of the external bootpin settings.

If I wipe the u-boot from eMMC, it will load the u-boot on the SD card if the external boot pins are

set to Mode0=1, Mode1=0

I expect the boot ROM is falling back to SD due to SDMMC_MFG (manufacture mode) still being active.

Page 824 defines further boot config registers:
 3035_0480 Value of OTP Bank2 Word0 (OCOTP_HW_OCOTP_BOOT_CFG1) 
 3035_0490 Value of OTP Bank2 Word1 (OCOTP_HW_OCOTP_BOOT_CFG2)
 3035_04A0 Value of OTP Bank2 Word2 (OCOTP_HW_OCOTP_BOOT_CFG3)
 3035_04B0 Value of OTP Bank2 Word3 (OCOTP_HW_OCOTP_BOOT_CFG4)
Page 817 -- 819 covers the register fields. The registers were not altered. The default values are:
u-boot=> fuse sense 2 0 4
  01000010 00000000 00000000 00000000

I didn't use the FastBoot option. 

Regards,
Frikkie

0 件の賞賛
返信

8,411件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello, 

The way that you are going to program the efuses depends on several things. Principally by the specs of your memory. However, to make boot from the eMMC you need to make sure that the BOOT_CFG[14:12] registers are configured as below to boot from MMC/eMMC:

BOOT_CFG[14:12] = 010

The other configurations like I said before, depends on your memory configuration. You can find the description of the register description of the efuses on chapter 6.2 of the reference manual.

Hope this information can help you.

Best regards,

Diego.

0 件の賞賛
返信

8,411件の閲覧回数
Sasamy
Contributor IV

Hello Diego Adrian Cuevas.

According to this patch and processor manual

https://patchwork.kernel.org/patch/10929005/

"The i.MX8MM is similar to i.MX6 processors in terms of addressing and clock
setup."

i.MX 8M Mini Applications Processor Reference Manual, Rev. 1, 03/2019

Table 6-49. Fusemap Descriptions, page 823

0x470[15:0] BOOT_CFG

eFuse burning manual for i.mx6

https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX/#calculating-fuse-bank-and-word

(0x470 - 0x400) / 0x10 = 7
7 / 8 = 0 and the remainder is 7

Bank = 0
Word = 7‍‍‍‍‍

it is correct for i.MX8MM BOOT_CFG?

Alexander

0 件の賞賛
返信

8,409件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信

8,409件の閲覧回数
Sasamy
Contributor IV

Hello,

It seems to me that both articles are not suitable for i.MX8M Mini.
We used the Bank and Word values from the processor manual.

What we wanted to burn:

0x470 [14-12] 010 - MMC / eMMC
0x470 [11-10] 10 - SD3

i.MX 8M Mini Applications Processor Reference Manual, Rev. 2, 08/2019

6.3.4.16 Value of OTP Bank1 Word3 (Boot Configuration Info.)
(OCOTP_HW_OCOTP_BOOT_CFG00)

Shadowed memory mapped access to OTP Bank 1, word 3.

Address: 3035_0000h base + 470h offset = 3035_0470h

Therefore, we used this command in u-boot:

u-boot=> fuse prog 1 3 0x00002800

rogramming bank 1 word 0x00000003 to 0x00002800...
Warning: Programming fuses is an irreversible operation!
This may brick your system.
Use this command only if you are sure of what you are doing!

Alexander

8,409件の閲覧回数
Yuri
NXP Employee
NXP Employee

To understand how to calculate the bank and word, using address: look at OCOTP memory map in

section 6.3.4 (OCOTP Memory Map/Register Definition) of i.MX 8M Mini Reference Manual,

Rev. 2, 08/2019 :

 

3035_0400 - Bank 0 Word 0

3035_0410 - Bank 0 Word 1

...

3035_0440 - Bank 1 Word 0

 

  So, formula is as following:

 

  Bank = (address - 0x400) / 0x40 ;

  Word = [(address - 0x400) % 0x40] / 0x10 ;

8,409件の閲覧回数
tarterkit_ru
Contributor III

Hello, thanks.

I see this chapter, in this chpater desctibe BOOT_CFG, BOOT_CFG1 etc

But uboot requre "<bank> <word>", i need to figure out the accordance between "<bank> <word>" and BOOT_CFG registers.

0 件の賞賛
返信