imx8m nano RMII mode configuration problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8m nano RMII mode configuration problem

646件の閲覧回数
Rolandash
Contributor I

Hi,

I am trying to config imx8m nano ethernet interface into RMII mode. However I have met problem on ETH REF CLK. 

I am using an external 50MHz crystal to feed clock into imx8m nano as eth ref clk.  

My dts file looks as below:

 

&fec1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_fec1_b>;
        phy-mode = "rmii";
	//phy-handle = <&ethphy0>;
        fsl,magic-packet;
        phy-reset-gpios = <&gpio4 22 GPIO_ACTIVE_LOW>;
        //phy-reset-duration = <25>;
        //phy-reset-post-delay = <100>;
	assigned-clock-parents = <&clk IMX8MN_SYS_PLL1_266M>,
				 <&clk IMX8MN_SYS_PLL2_100M>,
				 <&clk IMX8MN_SYS_PLL2_50M>,
				 <&clk IMX8MN_SYS_PLL2_50M>;
	assigned-clock-rates = <0>, <100000000>, <50000000>, <0>;
	status = "okay";

	fixed-link {
	    speed = <100>;
	    full-duplex;
	};

        /*mdio {
	    #address-cells = <1>;
	    #size-cells = <0>;

	    ethphy0: ethernet-phy@0 {
                compatible = "ethernet-phy-ieee802.3-c22";
                reg = <0>;
		max-speed = <100>;
	    };
        };*/
};

&iomuxc {

	pinctrl_fec1_b: fec1-bgrp {
		fsl,pins = <
			    MX8MN_IOMUXC_ENET_MDC_ENET1_MDC		0x03
			    MX8MN_IOMUXC_ENET_MDIO_ENET1_MDIO		0x23
			    MX8MN_IOMUXC_ENET_TD0_ENET1_RGMII_TD0	0x56
			    MX8MN_IOMUXC_ENET_TD1_ENET1_RGMII_TD1	0x56
			    MX8MN_IOMUXC_ENET_TD2_ENET1_TX_CLK		0x4000001f
			    MX8MN_IOMUXC_ENET_RD0_ENET1_RGMII_RD0	0x56 /* MODE0 */
			    MX8MN_IOMUXC_ENET_RD1_ENET1_RGMII_RD1	0x56 /* MODE1 */
			    MX8MN_IOMUXC_ENET_RXC_ENET1_RX_ER		0x110 /* PHYAD2 */
			    MX8MN_IOMUXC_ENET_RX_CTL_ENET1_RGMII_RX_CTL	0x56 /* CLK125_EN */
			    MX8MN_IOMUXC_ENET_TX_CTL_ENET1_RGMII_TX_CTL	0x56 /* LED_MODE */
		>;
	};

};

 

 

 

By this configuration I am expecting ENET_TD2 pad is muxed to be ref clk input.  

I try to verify the pin config after boot the system up by reading pad registers value using mem tool. All looks right but the IOMUXC_GPR_GPR1 register content.

According to the chip reference manual, the GPR_ENET1_ TX_CLK_SEL bit of this register is '0' by default, but now it reads "0x00002000", which means the ENET_TD2 pad been set to output of ref clk instead of input as I desired.

I did not change any other source code. So I am not sure why IOMUXC_GPR_GPR1 value is not as expected. Is there any other thing may change the value of this reg?

Please hint me if I missed something.

 

thank you very much.

 

/Roland

 

 

 

 

 

0 件の賞賛
返信
1 返信

594件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

You need modify setting in Uboot/board/freescale/imx8mn_evk/imx8mn_evk.c

Zhiming_Liu_0-1726032893900.png

Best Regards
Zhiming

0 件の賞賛
返信