I have an i.MX 8M Nano board. I want to attach a 5.5 inch WaveShare Screen 1920x1080 display panel as an output display but i cannot see anything except the initial charaters of NXP (in very dispersed order) and then screen appears black. When i connect the screen's touch interface with USB C port of Nano board. It continously output the following lines after every 4 or 5 seconds on COM port.

And when i connect the display after it boots up it shows the following lines but still nothing appears.

I have also tried without the touch interface but nothing seems to work. Moreover i have a DVI monitor and when i connect hdmi to dvi connector the monitor also shows nothing. I also tried to change the screen resolution according to monitor display ( video=HDMI-A-1:1280x1024-24@60) but still no success.
I am running "android_p9.0.0_2.3.1_image_8mnevk" image. Since i am new to this board please any help would be highly appreciated.